CircularGridBuilder Class |
Represents the circular grid section specifications for a NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisBuilder . |
CurveAlignedBuilder Class |
Represents the Curve Aligned specification for a NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilder . |
GridSpacingBuilder Class |
Represents the grid spacing for certain types of section specifications for the NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisBuilder . |
InteractiveBuilder Class |
Represents the Interactive specification for a NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilder . |
IsoparametricBuilder Class |
Represents the Isoparametric specification for a GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilder . |
ParallelPlanesExBuilder Class |
Represents the Parallel Plane specification for a GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilder . |
QuadrilateralGridBuilder Class |
Represents the quadrilateral grid section specifications for a GeometricAnalysis.SectionAnalysis.SectionAnalysisBuilder . |
RadialBuilder Class |
Represents the Radial specification for a GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilder . |
SectionAnalysisBuilder Class |
Represents a NXOpen.GeometricAnalysis.SectionAnalysisObject builder. |
SectionAnalysisExBuilder Class |
Represents a NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisExObject builder |
SectionAnalysisExObject Class |
Represents a Section Analysis Object of the new version. |
SectionPlaneBuilder Class |
Represents a plane which is used to cut sections on faces or facet bodies |
TriangularGridBuilder Class |
Represents the triangular grid section specifications for a SectionAnalysisBuilder. |
XYZPlaneBuilder Class |
Represents the XYZ Plane specification for a GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilder . |