SectionAnalysisExBuilderOutputType Enumeration¶
NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilder.OutputType is an alias for NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilderOutputType
-
class
NXOpen.GeometricAnalysis.SectionAnalysis.
SectionAnalysisExBuilderOutputType
¶ Bases:
object
The output options
Enum Members
Enum Member Enum Member Description AnalysisObject Analysis ObjectSectionCurves section curvesBoth Both Analysis Object and section curves-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-