SectionAnalysisBuilderCalculationMethodType Enumeration

NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisBuilder.CalculationMethodType is an alias for NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisBuilderCalculationMethodType

class NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisBuilderCalculationMethodType

Bases: object

The calculation method

Enum Members

Enum Member Enum Member Description
Curvature
Curvature
RadiusofCurvature
Radius of curvature
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.