CircularGridBuilder Class

class NXOpen.GeometricAnalysis.SectionAnalysis.CircularGridBuilder

Bases: NXOpen.TaggedObject, NXOpen.GeometricUtilities.IComponentBuilder

Represents the circular grid section specifications for a NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisBuilder.

Only used when type is NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisBuilderTypes.Circular.

New in version NX6.0.0.

Properties

Property Description
CircularFrame Returns the circular frame
Spacing Returns the spacing specification for the circular grid
SpecifiedPlane Returns the user specified section plane
Tag Returns the Tag for this object.

Methods

Method Description
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

CircularFrame

CircularGridBuilder.CircularFrame

Returns the circular frame

-------------------------------------

Getter Method

Signature CircularFrame()

Returns:
Return type:NXOpen.GeometricUtilities.CircularFrameBuilder

New in version NX6.0.0.

License requirements: studio_analyze (“STUDIO ANALYZE”)

Spacing

CircularGridBuilder.Spacing

Returns the spacing specification for the circular grid

-------------------------------------

Getter Method

Signature Spacing()

Returns:
Return type:NXOpen.GeometricAnalysis.SectionAnalysis.GridSpacingBuilder

New in version NX6.0.0.

License requirements: studio_analyze (“STUDIO ANALYZE”)

SpecifiedPlane

CircularGridBuilder.SpecifiedPlane

Returns the user specified section plane

-------------------------------------

Getter Method

Signature SpecifiedPlane()

Returns:
Return type:NXOpen.GeometricAnalysis.SectionAnalysis.SectionPlaneBuilder

New in version NX9.0.0.

License requirements: None.

Method Detail

Validate

CircularGridBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.