CurveAlignedBuilder Class¶
-
class
NXOpen.GeometricAnalysis.SectionAnalysis.
CurveAlignedBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents the Curve Aligned specification for a
NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilder
.New in version NX7.0.0.
Properties¶
Property | Description |
---|---|
Curves | Returns the curves |
IsSpacingEnabled | Returns or sets a value indicating whether the spacing is applied |
Number | Returns or sets a value indicating how many sections should be created |
Offset | Returns or sets a value indicating the distance from the start position |
Spacing | Returns or sets a value indicating the space between sections |
SpecifiedPlane | Returns the user specified project plane |
Tag | Returns the Tag for this object. |
UseProjectedCurve | Returns or sets a value indicating whether to project the curve to a plane |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Curves¶
-
CurveAlignedBuilder.
Curves
¶ Returns the curves
-------------------------------------
Getter Method
Signature
Curves()
Returns: Return type: NXOpen.ScCollector
New in version NX7.0.0.
License requirements: None.
IsSpacingEnabled¶
-
CurveAlignedBuilder.
IsSpacingEnabled
¶ Returns or sets a value indicating whether the spacing is applied
-------------------------------------
Getter Method
Signature
IsSpacingEnabled()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsSpacingEnabled(isSpacingEnabled)
Parameters: isSpacingEnabled (bool) – New in version NX7.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
Number¶
-
CurveAlignedBuilder.
Number
¶ Returns or sets a value indicating how many sections should be created
-------------------------------------
Getter Method
Signature
Number()
Returns: Return type: int New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Number(number)
Parameters: number (int) – New in version NX7.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
Offset¶
-
CurveAlignedBuilder.
Offset
¶ Returns or sets a value indicating the distance from the start position
-------------------------------------
Getter Method
Signature
Offset()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Offset(offset)
Parameters: offset (float) – New in version NX7.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
Spacing¶
-
CurveAlignedBuilder.
Spacing
¶ Returns or sets a value indicating the space between sections
-------------------------------------
Getter Method
Signature
Spacing()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Spacing(spacing)
Parameters: spacing (float) – New in version NX7.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
SpecifiedPlane¶
-
CurveAlignedBuilder.
SpecifiedPlane
¶ Returns the user specified project plane
-------------------------------------
Getter Method
Signature
SpecifiedPlane()
Returns: Return type: NXOpen.GeometricAnalysis.SectionAnalysis.SectionPlaneBuilder
New in version NX7.0.0.
License requirements: None.
UseProjectedCurve¶
-
CurveAlignedBuilder.
UseProjectedCurve
¶ Returns or sets a value indicating whether to project the curve to a plane
-------------------------------------
Getter Method
Signature
UseProjectedCurve()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseProjectedCurve(useProjectedCurve)
Parameters: useProjectedCurve (bool) – New in version NX7.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
Method Detail¶
Validate¶
-
CurveAlignedBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.