SectionAnalysisExBuilder Class¶
-
class
NXOpen.GeometricAnalysis.SectionAnalysis.
SectionAnalysisExBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisExObject
builderTo create a new instance of this class, use
NXOpen.GeometricAnalysis.AnalysisObjectCollection.CreateSectionAnalysisExBuilder()
Default values.
Property Value Alignment XYZPlane CalculationMethod Curvature CurveAligned.IsSpacingEnabled 0 CurveAligned.Number 5 CurveAligned.Offset 0 CurveAligned.Spacing 25 CurveAligned.SpecifiedPlane.Plane View CurveAligned.UseProjectedCurve 0 Interactive.IsCutInfiniteEnabled 0 IsShowInflectionPointsEnabled 0 IsShowLengthEnabled 0 IsShowPeakPointsEnabled 0 Isoparametric.IsSpacingEnabled 0 Isoparametric.IsUEnabled 1 Isoparametric.IsVEnabled 1 Isoparametric.Number 5 Isoparametric.Spacing 25 NeedleDirection Outside Output AnalysisObject ParallelPlanes.IsNumberEnabled 0 ParallelPlanes.IsSpacingEnabled 0 ParallelPlanes.Number 5 ParallelPlanes.Offset 0 ParallelPlanes.Spacing 50 (millimeters part), 2 (inches part) Placement Uniform Radial.IsSpacingEnabled 0 Radial.Number 5 Radial.Offset 0 Radial.RotationAxis View Radial.Spacing 72 ScalingMethod Linear XYZPlane.IsNumberEnabled 0 XYZPlane.IsSpacingEnabled 0 XYZPlane.IsXEnabled 1 XYZPlane.IsYEnabled 1 XYZPlane.IsZEnabled 1 XYZPlane.Number 5 XYZPlane.Spacing 50 (millimeters part), 2 (inches part) New in version NX7.0.0.
Properties¶
Property | Description |
---|---|
Alignment | Returns or sets the alignment type |
CalculationMethod | Returns or sets the calculation method |
CombOptions | Returns the comb options specification |
CurveAligned | Returns the Curve Aligned section specification. |
Interactive | Returns the Interactive placement specification. |
IsShowInflectionPointsEnabled | Returns or sets a value indicating whether to show the inflection points |
IsShowLengthEnabled | Returns or sets a value indicating whether to show the length of each section curve |
IsShowPeakPointsEnabled | Returns or sets a value indicating whether to show the peak points |
Isoparametric | Returns the Isoparametric section specification. |
NeedleDirection | Returns or sets the needle direction |
Output | Returns or sets the output |
ParallelPlanes | Returns the Parallel Planes section specification. |
Placement | Returns or sets the placement |
Radial | Returns the Radial section specification. |
ScalingMethod | Returns or sets the scaling method |
SelectObject | Returns the selected objects |
SpecifyPoint | Returns the specified points |
Tag | Returns the Tag for this object. |
XYZPlane | Returns the XYZ Planes section specification. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SectionAnalysisExBuilderAlignmentType Enumeration | The section alignment type |
SectionAnalysisExBuilderCalculationMethodType Enumeration | The calculation method |
SectionAnalysisExBuilderNeedleDirectionType Enumeration | The needle direction |
SectionAnalysisExBuilderOutputType Enumeration | The output options |
SectionAnalysisExBuilderPlacementType Enumeration | The types of the section placement |
SectionAnalysisExBuilderScalingMethodType Enumeration | The scaling method |
Property Detail¶
Alignment¶
-
SectionAnalysisExBuilder.
Alignment
¶ Returns or sets the alignment type
-------------------------------------
Getter Method
Signature
Alignment()
Returns: Return type: NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilderAlignmentType
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Alignment(alignment)
Parameters: alignment ( NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilderAlignmentType
) –New in version NX7.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
CalculationMethod¶
-
SectionAnalysisExBuilder.
CalculationMethod
¶ Returns or sets the calculation method
-------------------------------------
Getter Method
Signature
CalculationMethod()
Returns: Return type: NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilderCalculationMethodType
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CalculationMethod(calculationMethod)
Parameters: calculationMethod ( NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilderCalculationMethodType
) –New in version NX7.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
CombOptions¶
-
SectionAnalysisExBuilder.
CombOptions
¶ Returns the comb options specification
-------------------------------------
Getter Method
Signature
CombOptions()
Returns: Return type: NXOpen.GeometricUtilities.CombOptionsBuilder
New in version NX7.0.0.
License requirements: None.
CurveAligned¶
-
SectionAnalysisExBuilder.
CurveAligned
¶ Returns the Curve Aligned section specification.
Only used when type is
NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilderAlignmentType.CurveAligned
-------------------------------------
Getter Method
Signature
CurveAligned()
Returns: Return type: NXOpen.GeometricAnalysis.SectionAnalysis.CurveAlignedBuilder
New in version NX7.0.0.
License requirements: None.
Interactive¶
-
SectionAnalysisExBuilder.
Interactive
¶ Returns the Interactive placement specification.
Only used when type is
NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilderPlacementType.Interactive
-------------------------------------
Getter Method
Signature
Interactive()
Returns: Return type: NXOpen.GeometricAnalysis.SectionAnalysis.InteractiveBuilder
New in version NX7.0.0.
License requirements: None.
IsShowInflectionPointsEnabled¶
-
SectionAnalysisExBuilder.
IsShowInflectionPointsEnabled
¶ Returns or sets a value indicating whether to show the inflection points
-------------------------------------
Getter Method
Signature
IsShowInflectionPointsEnabled()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsShowInflectionPointsEnabled(inflection)
Parameters: inflection (bool) – New in version NX7.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
IsShowLengthEnabled¶
-
SectionAnalysisExBuilder.
IsShowLengthEnabled
¶ Returns or sets a value indicating whether to show the length of each section curve
-------------------------------------
Getter Method
Signature
IsShowLengthEnabled()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsShowLengthEnabled(length)
Parameters: length (bool) – New in version NX7.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
IsShowPeakPointsEnabled¶
-
SectionAnalysisExBuilder.
IsShowPeakPointsEnabled
¶ Returns or sets a value indicating whether to show the peak points
-------------------------------------
Getter Method
Signature
IsShowPeakPointsEnabled()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsShowPeakPointsEnabled(peak)
Parameters: peak (bool) – New in version NX7.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
Isoparametric¶
-
SectionAnalysisExBuilder.
Isoparametric
¶ Returns the Isoparametric section specification.
Only used when type is
NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilderAlignmentType.Isoparametric
-------------------------------------
Getter Method
Signature
Isoparametric()
Returns: Return type: NXOpen.GeometricAnalysis.SectionAnalysis.IsoparametricBuilder
New in version NX7.0.0.
License requirements: None.
NeedleDirection¶
-
SectionAnalysisExBuilder.
NeedleDirection
¶ Returns or sets the needle direction
-------------------------------------
Getter Method
Signature
NeedleDirection()
Returns: Return type: NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilderNeedleDirectionType
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NeedleDirection(needleDirection)
Parameters: needleDirection ( NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilderNeedleDirectionType
) –New in version NX7.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
Output¶
-
SectionAnalysisExBuilder.
Output
¶ Returns or sets the output
-------------------------------------
Getter Method
Signature
Output()
Returns: Return type: NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilderOutputType
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Output(output)
Parameters: output ( NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilderOutputType
) –New in version NX7.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
ParallelPlanes¶
-
SectionAnalysisExBuilder.
ParallelPlanes
¶ Returns the Parallel Planes section specification.
Only used when type is
NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilderAlignmentType.ParallelPlanes
-------------------------------------
Getter Method
Signature
ParallelPlanes()
Returns: Return type: NXOpen.GeometricAnalysis.SectionAnalysis.ParallelPlanesExBuilder
New in version NX7.0.0.
License requirements: None.
Placement¶
-
SectionAnalysisExBuilder.
Placement
¶ Returns or sets the placement
-------------------------------------
Getter Method
Signature
Placement()
Returns: Return type: NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilderPlacementType
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Placement(placement)
Parameters: placement ( NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilderPlacementType
) –New in version NX7.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
Radial¶
-
SectionAnalysisExBuilder.
Radial
¶ Returns the Radial section specification.
Only used when type is
NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilderAlignmentType.CurveAligned
-------------------------------------
Getter Method
Signature
Radial()
Returns: Return type: NXOpen.GeometricAnalysis.SectionAnalysis.RadialBuilder
New in version NX7.0.0.
License requirements: None.
ScalingMethod¶
-
SectionAnalysisExBuilder.
ScalingMethod
¶ Returns or sets the scaling method
-------------------------------------
Getter Method
Signature
ScalingMethod()
Returns: Return type: NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilderScalingMethodType
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ScalingMethod(scalingMethod)
Parameters: scalingMethod ( NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilderScalingMethodType
) –New in version NX7.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
SelectObject¶
-
SectionAnalysisExBuilder.
SelectObject
¶ Returns the selected objects
-------------------------------------
Getter Method
Signature
SelectObject()
Returns: Return type: NXOpen.SelectTaggedObjectList
New in version NX7.0.0.
License requirements: None.
SpecifyPoint¶
-
SectionAnalysisExBuilder.
SpecifyPoint
¶ Returns the specified points
-------------------------------------
Getter Method
Signature
SpecifyPoint()
Returns: Return type: NXOpen.SelectPointList
New in version NX7.0.0.
License requirements: None.
XYZPlane¶
-
SectionAnalysisExBuilder.
XYZPlane
¶ Returns the XYZ Planes section specification.
Only used when type is
NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilderAlignmentType.XYZPlane
-------------------------------------
Getter Method
Signature
XYZPlane()
Returns: Return type: NXOpen.GeometricAnalysis.SectionAnalysis.XYZPlaneBuilder
New in version NX7.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
SectionAnalysisExBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.