XYZPlaneBuilder Class

class NXOpen.GeometricAnalysis.SectionAnalysis.XYZPlaneBuilder

Bases: NXOpen.TaggedObject, NXOpen.GeometricUtilities.IComponentBuilder

Represents the XYZ Plane specification for a GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilder.

New in version NX7.0.0.

Properties

Property Description
AnchorOrigin Returns or sets the anchor position
AnchorXAxis Returns or sets the anchor X axis
AnchorYAxis Returns or sets the anchor Y axis
IsNumberEnabled Returns or sets a value indicating whether the number is used
IsSpacingEnabled Returns or sets a value indicating whether the spacing is applied
IsXEnabled Returns or sets a value indicating whether X is enabled
IsYEnabled Returns or sets a value indicating whether Y is enabled
IsZEnabled Returns or sets a value indicating whether Z is enabled
Number Returns or sets a value indicating how many sections should be created
Spacing Returns or sets a value indicating the space between sections
Tag Returns the Tag for this object.

Methods

Method Description
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

AnchorOrigin

XYZPlaneBuilder.AnchorOrigin

Returns or sets the anchor position

-------------------------------------

Getter Method

Signature AnchorOrigin()

Returns:
Return type:NXOpen.Point3d

New in version NX7.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature AnchorOrigin(anchorOrigin)

Parameters:anchorOrigin (NXOpen.Point3d) –

New in version NX7.0.0.

License requirements: studio_analyze (“STUDIO ANALYZE”)

AnchorXAxis

XYZPlaneBuilder.AnchorXAxis

Returns or sets the anchor X axis

-------------------------------------

Getter Method

Signature AnchorXAxis()

Returns:
Return type:NXOpen.Vector3d

New in version NX7.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature AnchorXAxis(anchorXAxis)

Parameters:anchorXAxis (NXOpen.Vector3d) –

New in version NX7.0.0.

License requirements: studio_analyze (“STUDIO ANALYZE”)

AnchorYAxis

XYZPlaneBuilder.AnchorYAxis

Returns or sets the anchor Y axis

-------------------------------------

Getter Method

Signature AnchorYAxis()

Returns:
Return type:NXOpen.Vector3d

New in version NX7.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature AnchorYAxis(anchorYAxis)

Parameters:anchorYAxis (NXOpen.Vector3d) –

New in version NX7.0.0.

License requirements: studio_analyze (“STUDIO ANALYZE”)

IsNumberEnabled

XYZPlaneBuilder.IsNumberEnabled

Returns or sets a value indicating whether the number is used

-------------------------------------

Getter Method

Signature IsNumberEnabled()

Returns:
Return type:bool

New in version NX7.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature IsNumberEnabled(isNumberEnabled)

Parameters:isNumberEnabled (bool) –

New in version NX7.0.0.

License requirements: studio_analyze (“STUDIO ANALYZE”)

IsSpacingEnabled

XYZPlaneBuilder.IsSpacingEnabled

Returns or sets a value indicating whether the spacing is applied

-------------------------------------

Getter Method

Signature IsSpacingEnabled()

Returns:
Return type:bool

New in version NX7.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature IsSpacingEnabled(isSpacingEnabled)

Parameters:isSpacingEnabled (bool) –

New in version NX7.0.0.

License requirements: studio_analyze (“STUDIO ANALYZE”)

IsXEnabled

XYZPlaneBuilder.IsXEnabled

Returns or sets a value indicating whether X is enabled

-------------------------------------

Getter Method

Signature IsXEnabled()

Returns:
Return type:bool

New in version NX7.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature IsXEnabled(isXEnabled)

Parameters:isXEnabled (bool) –

New in version NX7.0.0.

License requirements: studio_analyze (“STUDIO ANALYZE”)

IsYEnabled

XYZPlaneBuilder.IsYEnabled

Returns or sets a value indicating whether Y is enabled

-------------------------------------

Getter Method

Signature IsYEnabled()

Returns:
Return type:bool

New in version NX7.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature IsYEnabled(isYEnabled)

Parameters:isYEnabled (bool) –

New in version NX7.0.0.

License requirements: studio_analyze (“STUDIO ANALYZE”)

IsZEnabled

XYZPlaneBuilder.IsZEnabled

Returns or sets a value indicating whether Z is enabled

-------------------------------------

Getter Method

Signature IsZEnabled()

Returns:
Return type:bool

New in version NX7.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature IsZEnabled(isZEnabled)

Parameters:isZEnabled (bool) –

New in version NX7.0.0.

License requirements: studio_analyze (“STUDIO ANALYZE”)

Number

XYZPlaneBuilder.Number

Returns or sets a value indicating how many sections should be created

-------------------------------------

Getter Method

Signature Number()

Returns:
Return type:int

New in version NX7.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Number(number)

Parameters:number (int) –

New in version NX7.0.0.

License requirements: studio_analyze (“STUDIO ANALYZE”)

Spacing

XYZPlaneBuilder.Spacing

Returns or sets a value indicating the space between sections

-------------------------------------

Getter Method

Signature Spacing()

Returns:
Return type:float

New in version NX7.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Spacing(spacing)

Parameters:spacing (float) –

New in version NX7.0.0.

License requirements: studio_analyze (“STUDIO ANALYZE”)

Method Detail

Validate

XYZPlaneBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.