SectionAnalysisExBuilderPlacementType Enumeration

NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilder.PlacementType is an alias for NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilderPlacementType

class NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilderPlacementType

Bases: object

The types of the section placement

Enum Members

Enum Member Enum Member Description
Uniform
Uniformly distributed
ThroughPoints
Through the specified points
BetweenPoints
Distributed between two specified points
Interactive
Interactively specified
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.