SectionAnalysisExBuilderNeedleDirectionType Enumeration

NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilder.NeedleDirectionType is an alias for NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilderNeedleDirectionType

class NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilderNeedleDirectionType

Bases: object

The needle direction

Enum Members

Enum Member Enum Member Description
Inside
Inside
Outside
Outside
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.