SectionAnalysisExBuilderScalingMethodType Enumeration

NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilder.ScalingMethodType is an alias for NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilderScalingMethodType

class NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilderScalingMethodType

Bases: object

The scaling method

Enum Members

Enum Member Enum Member Description
Linear
Linear
Logarithmic
Logarithmic
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.