ParallelPlanesExBuilder Class¶
-
class
NXOpen.GeometricAnalysis.SectionAnalysis.
ParallelPlanesExBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents the Parallel Plane specification for a
GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilder
.New in version NX7.0.0.
Properties¶
Property | Description |
---|---|
IsNumberEnabled | Returns or sets a value indicating whether the number is used |
IsSpacingEnabled | Returns or sets a value indicating whether the spacing is applied |
Number | Returns or sets a value indicating how many sections should be created |
Offset | Returns or sets a value indicating the distance from the start position |
Spacing | Returns or sets a value indicating the space between sections |
SpecifiedPlane | Returns the user specified section plane |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
IsNumberEnabled¶
-
ParallelPlanesExBuilder.
IsNumberEnabled
¶ Returns or sets a value indicating whether the number is used
-------------------------------------
Getter Method
Signature
IsNumberEnabled()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsNumberEnabled(isNumberEnabled)
Parameters: isNumberEnabled (bool) – New in version NX7.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
IsSpacingEnabled¶
-
ParallelPlanesExBuilder.
IsSpacingEnabled
¶ Returns or sets a value indicating whether the spacing is applied
-------------------------------------
Getter Method
Signature
IsSpacingEnabled()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsSpacingEnabled(isSpacingEnabled)
Parameters: isSpacingEnabled (bool) – New in version NX7.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
Number¶
-
ParallelPlanesExBuilder.
Number
¶ Returns or sets a value indicating how many sections should be created
-------------------------------------
Getter Method
Signature
Number()
Returns: Return type: int New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Number(number)
Parameters: number (int) – New in version NX7.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
Offset¶
-
ParallelPlanesExBuilder.
Offset
¶ Returns or sets a value indicating the distance from the start position
-------------------------------------
Getter Method
Signature
Offset()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Offset(offset)
Parameters: offset (float) – New in version NX7.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
Spacing¶
-
ParallelPlanesExBuilder.
Spacing
¶ Returns or sets a value indicating the space between sections
-------------------------------------
Getter Method
Signature
Spacing()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Spacing(spacing)
Parameters: spacing (float) – New in version NX7.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
SpecifiedPlane¶
-
ParallelPlanesExBuilder.
SpecifiedPlane
¶ Returns the user specified section plane
-------------------------------------
Getter Method
Signature
SpecifiedPlane()
Returns: Return type: NXOpen.GeometricAnalysis.SectionAnalysis.SectionPlaneBuilder
New in version NX7.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
ParallelPlanesExBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.