SectionAnalysisExBuilderAlignmentType Enumeration

NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilder.AlignmentType is an alias for NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilderAlignmentType

class NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisExBuilderAlignmentType

Bases: object

The section alignment type

Enum Members

Enum Member Enum Member Description
XYZPlane
The cutting planes are perpendicular to X, Y or Z plane
ParallelPlanes
The cutting planes are parallel to a specified plane
CurveAligned
The cutting planes are perpendicular to specified curves
Isoparametric
The sections are along isoparametric lines
Radial
The cutting planes are distributed along a circle
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.