TriangularGridBuilder Class¶
-
class
NXOpen.GeometricAnalysis.SectionAnalysis.
TriangularGridBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents the triangular grid section specifications for a SectionAnalysisBuilder.
Only used when type is
GeometricAnalysis.SectionAnalysis.SectionAnalysisBuilderTypes.Triangular
.New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Spacing | Returns the spacing specification for the triangular grid |
SpecifiedPlane | Returns the user specified section plane |
Tag | Returns the Tag for this object. |
TriangularFrame | Returns the triangular frame |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Spacing¶
-
TriangularGridBuilder.
Spacing
¶ Returns the spacing specification for the triangular grid
-------------------------------------
Getter Method
Signature
Spacing()
Returns: Return type: NXOpen.GeometricAnalysis.SectionAnalysis.GridSpacingBuilder
New in version NX6.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
SpecifiedPlane¶
-
TriangularGridBuilder.
SpecifiedPlane
¶ Returns the user specified section plane
-------------------------------------
Getter Method
Signature
SpecifiedPlane()
Returns: Return type: NXOpen.GeometricAnalysis.SectionAnalysis.SectionPlaneBuilder
New in version NX9.0.0.
License requirements: None.
TriangularFrame¶
-
TriangularGridBuilder.
TriangularFrame
¶ Returns the triangular frame
-------------------------------------
Getter Method
Signature
TriangularFrame()
Returns: Return type: NXOpen.GeometricUtilities.TriangularFrameBuilder
New in version NX6.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
Method Detail¶
Validate¶
-
TriangularGridBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.