SectionAnalysisBuilderOutputType Enumeration

NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisBuilder.OutputType is an alias for NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisBuilderOutputType

class NXOpen.GeometricAnalysis.SectionAnalysis.SectionAnalysisBuilderOutputType

Bases: object

The output options

Enum Members

Enum Member Enum Member Description
AnalysisObject
Analysis Object
SectionCurves
section curves
Both
Both Analysis Object and section curves
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.