QuadrilateralGridBuilder Class

class NXOpen.GeometricAnalysis.SectionAnalysis.QuadrilateralGridBuilder

Bases: NXOpen.TaggedObject, NXOpen.GeometricUtilities.IComponentBuilder

Represents the quadrilateral grid section specifications for a GeometricAnalysis.SectionAnalysis.SectionAnalysisBuilder.

Only used when type is GeometricAnalysis.SectionAnalysis.SectionAnalysisBuilderTypes.Quadrilateral.

New in version NX6.0.0.

Properties

Property Description
QuadrilateralFrame Returns the quadrilateral frame
Spacing Returns the spacing specification for the quadrilateral grid
SpecifiedPlane Returns the user specified section plane
Tag Returns the Tag for this object.

Methods

Method Description
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

QuadrilateralFrame

QuadrilateralGridBuilder.QuadrilateralFrame

Returns the quadrilateral frame

-------------------------------------

Getter Method

Signature QuadrilateralFrame()

Returns:
Return type:NXOpen.GeometricUtilities.QuadrilateralFrameBuilder

New in version NX6.0.0.

License requirements: studio_analyze (“STUDIO ANALYZE”)

Spacing

QuadrilateralGridBuilder.Spacing

Returns the spacing specification for the quadrilateral grid

-------------------------------------

Getter Method

Signature Spacing()

Returns:
Return type:NXOpen.GeometricAnalysis.SectionAnalysis.GridSpacingBuilder

New in version NX6.0.0.

License requirements: studio_analyze (“STUDIO ANALYZE”)

SpecifiedPlane

QuadrilateralGridBuilder.SpecifiedPlane

Returns the user specified section plane

-------------------------------------

Getter Method

Signature SpecifiedPlane()

Returns:
Return type:NXOpen.GeometricAnalysis.SectionAnalysis.SectionPlaneBuilder

New in version NX9.0.0.

License requirements: None.

Method Detail

Validate

QuadrilateralGridBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.