SectionPlaneBuilderPlaneType Enumeration

NXOpen.GeometricAnalysis.SectionAnalysis.SectionPlaneBuilder.PlaneType is an alias for NXOpen.GeometricAnalysis.SectionAnalysis.SectionPlaneBuilderPlaneType

class NXOpen.GeometricAnalysis.SectionAnalysis.SectionPlaneBuilderPlaneType

Bases: object

The type of different section planes

Enum Members

Enum Member Enum Member Description
Xc
XC plane
Yc
YC plane
Zc
ZC plane
View
View plane
Plane
A user specifed plane
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.