CurveAnalysisCombsBuilderDirectionOptionType Enumeration |
Direction option types |
CurveAnalysisDisplayShowFlagType Enumeration |
Show flag types |
CurveAnalysisInflectionsBuilderDirectionOptionType Enumeration |
Direction option types |
CurveAnalysisPeaksBuilderDirectionOptionType Enumeration |
Direction option types |
CurveAnalysisRecordDirectionOptionType Enumeration |
Direction option types |
CurveCurvatureAnalysisBuilderCalculationMethod Enumeration |
Enumeration for needle calculation method |
CurveCurvatureAnalysisBuilderDisplayStyle Enumeration |
Enumeration for needle display type |
CurveCurvatureAnalysisBuilderLabelValues Enumeration |
Enumeration for label computation method |
CurveCurvatureAnalysisBuilderNeedleDirection Enumeration |
Enumeration for needle direction type |
CurveCurvatureAnalysisBuilderProjectionTypes Enumeration |
Projection plane types |
CurveCurvatureAnalysisBuilderXyzTypes Enumeration |
Enumeration for X, Y or Z projection plane |
DeviationCheckingDeviationOptions Enumeration |
the deviation type to be shown |
DeviationCheckingTypes Enumeration |
the type of deviation checking to be performed |
DeviationGaugeBuilderAdditionalValuesLabelType Enumeration |
This enum represents the Deviation Gauge Analysis Object additional values label type |
DeviationGaugeBuilderColorPlotTypes Enumeration |
This enum represents the Deviation Gauge Analysis Object color plot types |
DeviationGaugeBuilderMeasurementMethodType Enumeration |
This enum represents the Deviation Gauge Analysis Object evaluation types |
DeviationGaugeBuilderMinMaxType Enumeration |
This enum represents the Deviation Gauge Analysis Object min max type |
DeviationGaugeBuilderReportingPerTypes Enumeration |
This enum represents the Deviation Gauge Analysis Object reporting per setting |
DeviationGaugeBuilderXyzDirectionType Enumeration |
This enum represents the Deviation Gauge Analysis Object X, Y, Z direction options |
DistanceAnalysisBuilderDisplayModes Enumeration |
The display type. |
DraftAnalysisBuilderDrawDirection Enumeration |
define draw direction items |
DraftAnalysisBuilderSelectOutput Enumeration |
define output options |
ExamineGeometryCheck Enumeration |
Types of checks |
FaceAnalysisDisplayBuilderColorLegendOptions Enumeration |
Represents color legend type in display. |
FaceAnalysisDisplayBuilderColorsOptions Enumeration |
The option indicating number of colors to be used for display. |
FaceCurvatureAnalysisBuilderCurvatureTypes Enumeration |
Represents the face curvature types. |
FaceCurvatureAnalysisBuilderDirectionTypes Enumeration |
Methods of specifiying the direction for normal and section curvatures. |
FaceCurvatureAnalysisBuilderDisplayTypes Enumeration |
Represents the display types. |
FaceCurvatureAnalysisBuilderScaleTypes Enumeration |
Represents the scaling types for curvature values. |
GapFlushnessBuilderDisplayOptions Enumeration |
This enum represents Label Display Option type |
GapFlushnessBuilderEvaluationModes Enumeration |
This enum represents evaluation mode |
GapFlushnessBuilderEvaluationTypes Enumeration |
This enum represents the Gap and Flushness Analysis Object evaluation types |
GapFlushnessBuilderPanelTypes Enumeration |
This enum represents panel type |
GapFlushnessBuilderSectionAlignments Enumeration |
This enum represents cross-section alignment type |
GapFlushnessBuilderSectionCurveOptions Enumeration |
This enum represents Cross Section Curves Options |
GeometricPropertiesEntity Enumeration |
Type of input entity for geometric properties. |
GeometricPropertiesOutputType Enumeration |
Represents how to output geometric properties. |
GeometricPropertiesStatus Enumeration |
Status of computing geometric properties. |
HighlightLinesAnalysisBuilderDisplayMethods Enumeration |
display methods |
HighlightLinesAnalysisBuilderLightPlacements Enumeration |
light placement |
HighlightLinesAnalysisBuilderLightPlaneOptions Enumeration |
light plane options |
HighlightLinesAnalysisBuilderResolutions Enumeration |
resolution options |
HighlightLinesAnalysisBuilderTypes Enumeration |
three types of light methods |
HighlightLinesAnalysisBuilderTypes2 Enumeration |
four types of display methods |
RadiusAnalysisBuilderDisplayModes Enumeration |
The display type. |
RadiusAnalysisBuilderTypes Enumeration |
Represents the radius type. |
ReflectionAnalysisBuilderImageMovementTypes Enumeration |
The type of image movement. |
ReflectionAnalysisBuilderImageSizeOption Enumeration |
The reflection image size option. |
ReflectionAnalysisBuilderLineImageTypes Enumeration |
The line image types. |
ReflectionAnalysisBuilderLineOrientationType Enumeration |
The reflection line orientation. |
ReflectionAnalysisBuilderLineThicknessType Enumeration |
The reflection line thickness. |
ReflectionAnalysisBuilderNumberOfLinesOptions Enumeration |
The number of reflection lines. |
ReflectionAnalysisBuilderSceneImageType Enumeration |
The reflection scene images. |
ReflectionAnalysisBuilderTypes Enumeration |
The types of images. |
SimpleInterferenceFaceInterferenceMethod Enumeration |
Specifies to find only first pair of interfering faces or all pairs of interfering faces between the input boides. |
SimpleInterferenceInterferenceMethod Enumeration |
Specifies interference method, i. |
SimpleInterferenceResult Enumeration |
Specifies the result of a simple interference check |
SlopeAnalysisBuilderDisplayModes Enumeration |
The display type. |
SolidDensityUnitsType Enumeration |
Types of units for solid density |
SurfaceAnalysisDisplayShowFlagType Enumeration |
Show flag types |
SurfaceContinuityAnalysisBuilderCurvatureType Enumeration |
Curvature types |
SurfaceContinuityAnalysisBuilderReportingType Enumeration |
Reporting types |
SurfaceContinuityAnalysisBuilderTypes Enumeration |
Two possible types for the dialog |
SurfaceIntersectionBuilderCalculationTypes Enumeration |
Enumeration for needle calculation method |
SurfaceIntersectionBuilderDirectionTypes Enumeration |
Enumeration for needle direction type |
SurfaceIntersectionBuilderLabelValues Enumeration |
Enumeration for label computation method |
SurfaceIntersectionBuilderNormalTypes Enumeration |
Enumeration for face normal |
SurfaceIntersectionBuilderProjectionTypes Enumeration |
Projection types |
SurfaceIntersectionBuilderScalingTypes Enumeration |
Enumeration for needle display type |
SurfaceIntersectionBuilderXyzTypes Enumeration |
Enumeration for X, Y or Z projection plane |