FaceAnalysisDisplayBuilderColorsOptions Enumeration¶
NXOpen.GeometricAnalysis.FaceAnalysisDisplayBuilder.ColorsOptions is an alias for NXOpen.GeometricAnalysis.FaceAnalysisDisplayBuilderColorsOptions
-
class
NXOpen.GeometricAnalysis.
FaceAnalysisDisplayBuilderColorsOptions
¶ Bases:
object
The option indicating number of colors to be used for display.
Enum Members
Enum Member Enum Member Description Two Display in 2 colors.Three Display in 3 colors.Four Display in 4 colors.Five Display in 5 colors.Six Display in 6 colors.Seven Display in 7 colors.Eight Display in 8 colors.Nine Display in 9 colors.Ten Display in 10 colors.Eleven Display in 11 colors.Twelve Display in 12 colors.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-