HighlightLinesAnalysisBuilderLightPlaneOptions Enumeration¶
NXOpen.GeometricAnalysis.HighlightLinesAnalysisBuilder.LightPlaneOptions is an alias for NXOpen.GeometricAnalysis.HighlightLinesAnalysisBuilderLightPlaneOptions
-
class
NXOpen.GeometricAnalysis.
HighlightLinesAnalysisBuilderLightPlaneOptions
¶ Bases:
object
light plane options
Enum Members
Enum Member Enum Member Description YZ Uses YC-ZC plane as light planeZX Uses XC-ZC plane as light planeXY Uses XC-YC plane as light planeArbitrary Uses an arbitrary plane as light plane-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-