FaceAnalysisNormalsBuilder Class¶
-
class
NXOpen.GeometricAnalysis.
FaceAnalysisNormalsBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents reverse normal functions used by Face Analysis.
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
FaceToReverseNormal | Returns the face to reverse normal |
Point | Returns or sets the point to redirect normals |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
FaceToReverseNormal¶
-
FaceAnalysisNormalsBuilder.
FaceToReverseNormal
¶ Returns the face to reverse normal
-------------------------------------
Getter Method
Signature
FaceToReverseNormal()
Returns: Return type: NXOpen.SelectNXObject
New in version NX11.0.0.
License requirements: None.
Point¶
-
FaceAnalysisNormalsBuilder.
Point
¶ Returns or sets the point to redirect normals
-------------------------------------
Getter Method
Signature
Point()
Returns: Return type: NXOpen.Point
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Point(point)
Parameters: point ( NXOpen.Point
) –New in version NX11.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
FaceAnalysisNormalsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.