SurfaceIntersectionBuilderXyzTypes Enumeration¶
NXOpen.GeometricAnalysis.SurfaceIntersectionBuilder.XyzTypes is an alias for NXOpen.GeometricAnalysis.SurfaceIntersectionBuilderXyzTypes
-
class
NXOpen.GeometricAnalysis.
SurfaceIntersectionBuilderXyzTypes
¶ Bases:
object
Enumeration for X, Y or Z projection plane
Enum Members
Enum Member Enum Member Description X x-axis planeY y-axis planeZ z-axis plane-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-