ReflectionAnalysisBuilderLineImageTypes Enumeration¶
NXOpen.GeometricAnalysis.ReflectionAnalysisBuilder.LineImageTypes is an alias for NXOpen.GeometricAnalysis.ReflectionAnalysisBuilderLineImageTypes
-
class
NXOpen.GeometricAnalysis.
ReflectionAnalysisBuilderLineImageTypes
¶ Bases:
object
The line image types.
Enum Members
Enum Member Enum Member Description BlackLines Black lines.BlackandWhiteLines Black and lines.ColoredLines Colored lines.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-