DeviationCheckingTypes Enumeration¶
NXOpen.GeometricAnalysis.DeviationChecking.Types is an alias for NXOpen.GeometricAnalysis.DeviationCheckingTypes
-
class
NXOpen.GeometricAnalysis.
DeviationCheckingTypes
¶ Bases:
object
the type of deviation checking to be performed
Enum Members
- curve/edge to curve/edge deviation “
- “CurveToFace”, ” check curve/edge
- to face deviation “
- “EdgeToFace”, ” check edge to face
- deviation “
- “FaceToFace”, ” check face to face
- deviation “
- “EdgeToEdge”, ” check edge to edge
deviation “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.