SolidDensityUnitsType Enumeration¶
NXOpen.GeometricAnalysis.SolidDensity.UnitsType is an alias for NXOpen.GeometricAnalysis.SolidDensityUnitsType
-
class
NXOpen.GeometricAnalysis.
SolidDensityUnitsType
¶ Bases:
object
Types of units for solid density
Enum Members
Enum Member Enum Member Description PoundsPerCubicInches Lbs/Cubic InchesPoundsPerCubicFeet Lbs/Cubic FeetGramsPerCubicCentimeters Grams/Cubic CentimetersKilogramsPerCubicMeters Kilograms/Cubic Meters-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-