ExamineGeometryCheck Enumeration¶
NXOpen.GeometricAnalysis.ExamineGeometry.Check is an alias for NXOpen.GeometricAnalysis.ExamineGeometryCheck
-
class
NXOpen.GeometricAnalysis.
ExamineGeometryCheck
¶ Bases:
object
Types of checks
Enum Members
Enum Member Enum Member Description ObjectTiny ObjectTinyObjectMisaligned ObjectMisalignedBodyDataStructures BodyDataStructuresBodyConsistency BodyConsistencyBodyFaceIntersections BodyFaceIntersectionsBodySheetBoundaries BodySheetBoundariesFaceSmoothness FaceSmoothnessFaceSelfIntersection FaceSelfIntersectionFaceSpikesCuts FaceSpikesCutsEdgeSmoothness EdgeSmoothnessEdgeTolerances EdgeTolerancesNumChecks Number of Checks-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-