DupinBuilder Class¶
-
class
NXOpen.GeometricAnalysis.
DupinBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
The Dupin Indicatrix is a tool to geometrically display the surface curvature at a specified point on a surface.
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
AnalysisPoint | Returns or sets the point location defining where the analysis should be done. |
Angle | Returns or sets the deviation in degrees from the minimum curvature. |
FlatnessTolerance | Returns or sets the tolerance that defines at the specified point if an area is flat. |
Scale | Returns or sets the scale factor to apply to the display of the dupin indicatrix. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
ResetAnalysisPoint | Reset the analysis point to accept dynamic input. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AnalysisPoint¶
-
DupinBuilder.
AnalysisPoint
¶ Returns or sets the point location defining where the analysis should be done.
-------------------------------------
Getter Method
Signature
AnalysisPoint()
Returns: Return type: NXOpen.Point
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AnalysisPoint(analysisPoint)
Parameters: analysisPoint ( NXOpen.Point
) –New in version NX8.0.0.
License requirements: None.
Angle¶
-
DupinBuilder.
Angle
¶ Returns or sets the deviation in degrees from the minimum curvature.
This value is used to rotate the normal curvature about the specified point.
-------------------------------------
Getter Method
Signature
Angle()
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Angle(angle)
Parameters: angle (float) – New in version NX8.0.0.
License requirements: None.
FlatnessTolerance¶
-
DupinBuilder.
FlatnessTolerance
¶ Returns or sets the tolerance that defines at the specified point if an area is flat.
-------------------------------------
Getter Method
Signature
FlatnessTolerance()
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FlatnessTolerance(flatnessTolerance)
Parameters: flatnessTolerance (float) – New in version NX8.0.0.
License requirements: None.
Scale¶
-
DupinBuilder.
Scale
¶ Returns or sets the scale factor to apply to the display of the dupin indicatrix.
-------------------------------------
Getter Method
Signature
Scale()
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Scale(scale)
Parameters: scale (float) – New in version NX8.0.0.
License requirements: None.
Method Detail¶
ResetAnalysisPoint¶
-
DupinBuilder.
ResetAnalysisPoint
¶ Reset the analysis point to accept dynamic input.
Signature
ResetAnalysisPoint()
New in version NX8.0.0.
License requirements: None.
Validate¶
-
DupinBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.