ReflectionAnalysisBuilder Class¶
-
class
NXOpen.GeometricAnalysis.
ReflectionAnalysisBuilder
¶ Bases:
NXOpen.Builder
Represents a Reflection Analysis builder.
To create a new instance of this class, use
NXOpen.GeometricAnalysis.AnalysisObjectCollectionEx.CreateReflectionAnalysisBuilder()
Default values.
Property Value DisplayResolution.AngleTolerance 15.0 DisplayResolution.EdgeTolerance 0.005 DisplayResolution.FaceTolerance 0.005 DisplayResolution.Resolution Standard DisplayResolution.WidthTolerance 0.3 FaceReflectivityScale 100 ImagePosition 0 LineNumber ThirtyTwo ShowFacetEdge 0 New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
DisplayResolution | Returns the display resolution. |
FaceReflectivityScale | Returns or sets the face reflectivity scale from 0 to 100. |
Faces | Returns the face to apply reflection analysis. |
FileName | Returns or sets the file browser. |
ImageMovementType | Returns or sets the orientation to move reflection lines. |
ImagePosition | Returns or sets the moving image scale. |
ImageSizeSetting | Returns or sets the image size setting. |
LineImageType | Returns or sets the image type. |
LineNumber | Returns or sets the reflection line number. |
LineOrientation | Returns or sets the reflection line orientation. |
LineThickness | Returns or sets the reflection line thickness. |
Normals | Returns the reflection analysis normals. |
SceneImageOption | Returns or sets the scene image option. |
ShowFacetEdge | Returns or sets the flag indicating if facet edges should be shown. |
Tag | Returns the Tag for this object. |
Type | Returns or sets the reflection analysis type. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
StartReflectionAnalysis | Start reflection analysis. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ReflectionAnalysisBuilderImageMovementTypes Enumeration | The type of image movement. |
ReflectionAnalysisBuilderImageSizeOption Enumeration | The reflection image size option. |
ReflectionAnalysisBuilderLineImageTypes Enumeration | The line image types. |
ReflectionAnalysisBuilderLineOrientationType Enumeration | The reflection line orientation. |
ReflectionAnalysisBuilderLineThicknessType Enumeration | The reflection line thickness. |
ReflectionAnalysisBuilderNumberOfLinesOptions Enumeration | The number of reflection lines. |
ReflectionAnalysisBuilderSceneImageType Enumeration | The reflection scene images. |
ReflectionAnalysisBuilderTypes Enumeration | The types of images. |
Property Detail¶
DisplayResolution¶
-
ReflectionAnalysisBuilder.
DisplayResolution
¶ Returns the display resolution.
-------------------------------------
Getter Method
Signature
DisplayResolution()
Returns: Return type: NXOpen.GeometricUtilities.DisplayResolutionBuilder
New in version NX11.0.0.
License requirements: None.
FaceReflectivityScale¶
-
ReflectionAnalysisBuilder.
FaceReflectivityScale
¶ Returns or sets the face reflectivity scale from 0 to 100.
-------------------------------------
Getter Method
Signature
FaceReflectivityScale()
Returns: Return type: int New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FaceReflectivityScale(faceReflectivityScale)
Parameters: faceReflectivityScale (int) – New in version NX11.0.0.
License requirements: None.
Faces¶
-
ReflectionAnalysisBuilder.
Faces
¶ Returns the face to apply reflection analysis.
-------------------------------------
Getter Method
Signature
Faces()
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX11.0.0.
License requirements: None.
FileName¶
-
ReflectionAnalysisBuilder.
FileName
¶ Returns or sets the file browser.
-------------------------------------
Getter Method
Signature
FileName()
Returns: Return type: str New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FileName(filename)
Parameters: filename (str) – New in version NX11.0.0.
License requirements: None.
ImageMovementType¶
-
ReflectionAnalysisBuilder.
ImageMovementType
¶ Returns or sets the orientation to move reflection lines.
-------------------------------------
Getter Method
Signature
ImageMovementType()
Returns: Return type: NXOpen.GeometricAnalysis.ReflectionAnalysisBuilderImageMovementTypes
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ImageMovementType(imageMovementType)
Parameters: imageMovementType ( NXOpen.GeometricAnalysis.ReflectionAnalysisBuilderImageMovementTypes
) –New in version NX11.0.0.
License requirements: None.
ImagePosition¶
-
ReflectionAnalysisBuilder.
ImagePosition
¶ Returns or sets the moving image scale.
-------------------------------------
Getter Method
Signature
ImagePosition()
Returns: Return type: int New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ImagePosition(imagePosition)
Parameters: imagePosition (int) – New in version NX11.0.0.
License requirements: None.
ImageSizeSetting¶
-
ReflectionAnalysisBuilder.
ImageSizeSetting
¶ Returns or sets the image size setting.
-------------------------------------
Getter Method
Signature
ImageSizeSetting()
Returns: Return type: NXOpen.GeometricAnalysis.ReflectionAnalysisBuilderImageSizeOption
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ImageSizeSetting(imageSizeSetting)
Parameters: imageSizeSetting ( NXOpen.GeometricAnalysis.ReflectionAnalysisBuilderImageSizeOption
) –New in version NX11.0.0.
License requirements: None.
LineImageType¶
-
ReflectionAnalysisBuilder.
LineImageType
¶ Returns or sets the image type.
-------------------------------------
Getter Method
Signature
LineImageType()
Returns: Return type: NXOpen.GeometricAnalysis.ReflectionAnalysisBuilderLineImageTypes
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LineImageType(lineImageType)
Parameters: lineImageType ( NXOpen.GeometricAnalysis.ReflectionAnalysisBuilderLineImageTypes
) –New in version NX11.0.0.
License requirements: None.
LineNumber¶
-
ReflectionAnalysisBuilder.
LineNumber
¶ Returns or sets the reflection line number.
-------------------------------------
Getter Method
Signature
LineNumber()
Returns: Return type: NXOpen.GeometricAnalysis.ReflectionAnalysisBuilderNumberOfLinesOptions
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LineNumber(lineNumber)
Parameters: lineNumber ( NXOpen.GeometricAnalysis.ReflectionAnalysisBuilderNumberOfLinesOptions
) –New in version NX11.0.0.
License requirements: None.
LineOrientation¶
-
ReflectionAnalysisBuilder.
LineOrientation
¶ Returns or sets the reflection line orientation.
-------------------------------------
Getter Method
Signature
LineOrientation()
Returns: Return type: NXOpen.GeometricAnalysis.ReflectionAnalysisBuilderLineOrientationType
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LineOrientation(lineOrientation)
Parameters: lineOrientation ( NXOpen.GeometricAnalysis.ReflectionAnalysisBuilderLineOrientationType
) –New in version NX11.0.0.
License requirements: None.
LineThickness¶
-
ReflectionAnalysisBuilder.
LineThickness
¶ Returns or sets the reflection line thickness.
-------------------------------------
Getter Method
Signature
LineThickness()
Returns: Return type: NXOpen.GeometricAnalysis.ReflectionAnalysisBuilderLineThicknessType
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LineThickness(lineThickness)
Parameters: lineThickness ( NXOpen.GeometricAnalysis.ReflectionAnalysisBuilderLineThicknessType
) –New in version NX11.0.0.
License requirements: None.
Normals¶
-
ReflectionAnalysisBuilder.
Normals
¶ Returns the reflection analysis normals.
-------------------------------------
Getter Method
Signature
Normals()
Returns: Return type: NXOpen.GeometricAnalysis.FaceAnalysisNormalsBuilder
New in version NX11.0.0.
License requirements: None.
SceneImageOption¶
-
ReflectionAnalysisBuilder.
SceneImageOption
¶ Returns or sets the scene image option.
-------------------------------------
Getter Method
Signature
SceneImageOption()
Returns: Return type: NXOpen.GeometricAnalysis.ReflectionAnalysisBuilderSceneImageType
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SceneImageOption(sceneImageOption)
Parameters: sceneImageOption ( NXOpen.GeometricAnalysis.ReflectionAnalysisBuilderSceneImageType
) –New in version NX11.0.0.
License requirements: None.
ShowFacetEdge¶
-
ReflectionAnalysisBuilder.
ShowFacetEdge
¶ Returns or sets the flag indicating if facet edges should be shown.
-------------------------------------
Getter Method
Signature
ShowFacetEdge()
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowFacetEdge(showFacetEdge)
Parameters: showFacetEdge (bool) – New in version NX11.0.0.
License requirements: None.
Type¶
-
ReflectionAnalysisBuilder.
Type
¶ Returns or sets the reflection analysis type.
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.GeometricAnalysis.ReflectionAnalysisBuilderTypes
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.GeometricAnalysis.ReflectionAnalysisBuilderTypes
) –New in version NX11.0.0.
License requirements: None.
Method Detail¶
StartReflectionAnalysis¶
-
ReflectionAnalysisBuilder.
StartReflectionAnalysis
¶ Start reflection analysis.
Signature
StartReflectionAnalysis()
New in version NX11.0.0.
License requirements: None.
Validate¶
-
ReflectionAnalysisBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.