SimpleInterferenceFaceInterferenceMethod Enumeration¶
NXOpen.GeometricAnalysis.SimpleInterference.FaceInterferenceMethod is an alias for NXOpen.GeometricAnalysis.SimpleInterferenceFaceInterferenceMethod
-
class
NXOpen.GeometricAnalysis.
SimpleInterferenceFaceInterferenceMethod
¶ Bases:
object
Specifies to “find only first pair of interfering faces” or “all pairs of interfering faces” between the input boides.
Enum Members
all pairs of interfering faces. “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-