GeometricPropertiesEntity Enumeration¶
NXOpen.GeometricAnalysis.GeometricProperties.Entity is an alias for NXOpen.GeometricAnalysis.GeometricPropertiesEntity
-
class
NXOpen.GeometricAnalysis.
GeometricPropertiesEntity
¶ Bases:
object
Type of input entity for geometric properties.
Enum Members
Enum Member Enum Member Description Face FaceEdge Either a modeling edge or a curve.CaeFace CAE FaceCaeCurve CAE Curve-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-