DeviationCheckingDeviationOptions Enumeration¶
NXOpen.GeometricAnalysis.DeviationChecking.DeviationOptions is an alias for NXOpen.GeometricAnalysis.DeviationCheckingDeviationOptions
-
class
NXOpen.GeometricAnalysis.
DeviationCheckingDeviationOptions
¶ Bases:
object
the deviation type to be shown
Enum Members
- deviations “
- “AllDeviations”, ” show all
- deviations “
- “MaximumDistance”, ” show
- maximum distance deviation “
- “MinimumDistance”, ” show
- minimum distance deviation “
- “MaximumAngle”, ” show maximum
- angle deviation “
- “MinimumAngle”, ” show minimum
angle deviation “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.