MillCutParameters Class¶
-
class
NXOpen.CAM.
MillCutParameters
¶ Bases:
NXOpen.CAM.CutParameters
Represents a
NXOpen.CAM.MillCutParameters
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
AcrossVoids | Returns the across voids |
ActionWhenGouging | Returns or sets the action when gouging |
AdjacentBlades | Returns or sets the Adjacent Blades Stock Option Type |
AllowUndercutting | Returns or sets the allow undercutting toggle |
ApplyToLastPass | Returns or sets the status for doing Blank Sensitive finish on the last cut level |
BladeStock | Returns the blade stock |
BlankDistance | Returns the blank distance |
BlankOverhang | Returns the blank overhang (inheritable tool dependent). |
BlankStock | Returns the blank stock |
BlendStock | Returns the blend stock |
BoundaryApproximation | Returns or sets the boundary approximation toggle |
BoundaryInTol | Returns or sets the boundary intol |
BoundaryOutTol | Returns or sets the boundary out tol |
BoundaryStock | Returns or sets the boundary stock |
CheckIpwCollisions | Returns or sets the value to Check for Ipw Collsions |
CheckSafeClearance | Returns the Check Safe Clearance |
CheckStock | Returns the check stock |
CleanupOutput | Returns the Cleanup Output |
CleanupSettings | Returns the Cleanup Settings |
CornerControl | Returns the corner control |
CornerFindingOptions | Returns or sets the Corner Finding Options |
CutAngle | Returns the cut angle |
CutAreaExtensionDistance | Returns the cut area extension distance builder |
CutBelowOverhangingBlank | Returns or sets the Cut Below Overhanging Blank Method |
CutBelowToolContact | Returns or sets the cut below tool contact setting |
CutBetweenLevels | Returns or sets the cut between levels |
CutDirection | Returns the cut direction |
CutOrder | Returns or sets the cut order |
CutWallsOnly | Returns or sets the Cut Walls Only toggle |
ExtendAcrossUndercut | Returns or sets the extend across undercut toggle |
ExtendAtEdges | Returns the Extend At Edges |
ExtendFloorTo | Returns or sets the extend floor to |
ExtendToPart | Returns or sets the extend to part flag |
FinishPasses | Returns the finish passes |
FloorSameAsPartStock | Returns or sets the floor same as part stock |
FloorStock | Returns the floor stock |
FollowCheck | Returns or sets the follow check geometry status |
FromLeadingEdge | Returns the from leading edge |
FromTrailingEdge | Returns the from trailing edge |
GlobalOptimization | Returns or sets the global optimzation status |
HolderClearance | Returns the Holder Clearance |
HubStock | Returns the hub stock |
IncludeBodiesOfSurfaceRegion | Returns or sets the flag to check bodies of surface region |
IpwType | Returns or sets the IPW type |
LevelToLevel | Returns the Level to Level |
LowerLimit | Returns the lower limit |
MaxCutStep | Returns the maximum cut step |
MaxCutTraverse | Returns the max cut traverse |
MergeDistance | Returns the merge distance builder (tool dependent double) |
MinCutVolume | Returns the minimum cut volume |
MinMaterialThickness | Returns the minimum material thickness |
MinimizeNumberOfEngages | Returns or sets the minimize number of engages toggle |
MultiDepthCut | Returns the Multi Depth Cut |
NeckClearance | Returns the Neck Clearance |
OutputUncutRegions | Returns the output uncut regions |
PartSafeClearance | Returns the Part Safe Clearance |
PartStock | Returns the part stock |
PartStockOffset | Returns the part stock offset |
PatternDirection | Returns or sets the pattern direction |
PlungeDirection | Returns or sets the plunge direction |
PreventUndercutting | Returns or sets the prevent undercutting toggle |
RegionConnection | Returns or sets the region connection |
RegionSequencing | Returns or sets the region resequencing |
RollToolOverEdges | Returns or sets the roll tool over edges toggle |
RotaryMaxAngleLimit | Returns or sets the rotary max angle limit |
RotaryMinAngleLimit | Returns or sets the min angle from part axis |
SelfIntersection | Returns or sets the Standard Drive Self-Intersect Status |
ShankClearance | Returns the Shank Clearance |
ShroudStock | Returns the shroud stock |
SimplifyShapes | Returns or sets the Simplify Shapes Method |
SinglePassOffset | Returns the Single Pass Offset |
SmallAreaAvoidance | Returns the small area avoidance |
SteepContainment | Returns the steep containment |
Stepover | Returns the stepover |
StepoverLimit | Returns the Stepover Limit |
Tag | Returns the Tag for this object. |
TextDepth | Returns the Text Depth |
TlaxisBladeRollAngle | Returns or sets the max blade roll angle |
Tolerances | Returns the Tolerances builder |
TolerantMachining | Returns or sets the tolerant machining status |
ToolAxisChange | Returns the tool axis change |
ToolAxisSmoothing | Returns or sets the degree of tool axis smoothing |
ToolAxisTilt | Returns the tool axis tilt |
ToolRunOff | Returns the Tool Run Off |
ToolRunOffType | Returns or sets the Tool Run Off Type |
ToolRunOn | Returns the Tool Run On |
ToolpathSmoothing | Returns or sets the degree of tool path smoothing |
TraverseOpenPasses | Returns or sets the open passes |
TrimControl | Returns or sets the trim control method type |
TrimStock | Returns the trim stock |
TrochoidalSettings | Returns the Trochoidal Settings |
UpDownCutting | Returns the up down cutting |
UsePrevious2dIpw | Returns or sets the use previous IPW toggle |
UseToolHolder | Returns or sets the use tool holder |
ValleyOverlapDistance | Returns the valley overlap distance |
WallStock | Returns the wall stock |
ZAxisSmoothing | Returns the Z Axis Smoothing. |
Methods¶
Property Detail¶
AcrossVoids¶
-
MillCutParameters.
AcrossVoids
¶ Returns the across voids
-------------------------------------
Getter Method
Signature
AcrossVoids()
Returns: Return type: NXOpen.CAM.AcrossVoids
New in version NX6.0.0.
License requirements: None.
ActionWhenGouging¶
-
MillCutParameters.
ActionWhenGouging
¶ Returns or sets the action when gouging
-------------------------------------
Getter Method
Signature
ActionWhenGouging()
Returns: the When Gouging Check value Return type: NXOpen.CAM.CutParametersActionWhenGougingTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ActionWhenGouging(propValue)
Parameters: propValue ( NXOpen.CAM.CutParametersActionWhenGougingTypes
) – the When Gouging Check valueNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
AdjacentBlades¶
-
MillCutParameters.
AdjacentBlades
¶ Returns or sets the Adjacent Blades Stock Option Type
-------------------------------------
Getter Method
Signature
AdjacentBlades()
Returns: the adjacent blades stock option type Return type: NXOpen.CAM.CutParametersAdjacentBladesTypes
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AdjacentBlades(adjacentBlades)
Parameters: adjacentBlades ( NXOpen.CAM.CutParametersAdjacentBladesTypes
) – the adjacent blades stock option typeNew in version NX8.5.0.
License requirements: cam_base (“CAM BASE”)
AllowUndercutting¶
-
MillCutParameters.
AllowUndercutting
¶ Returns or sets the allow undercutting toggle
-------------------------------------
Getter Method
Signature
AllowUndercutting()
Returns: the Undercut Handle Flag Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AllowUndercutting(propValue)
Parameters: propValue (bool) – the Undercut Handle Flag New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
ApplyToLastPass¶
-
MillCutParameters.
ApplyToLastPass
¶ Returns or sets the status for doing Blank Sensitive finish on the last cut level
-------------------------------------
Getter Method
Signature
ApplyToLastPass()
Returns: apply to last pass status Return type: bool New in version NX7.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
ApplyToLastPass(applyLastPassStatus)
Parameters: applyLastPassStatus (bool) – apply to last pass status New in version NX7.5.1.
License requirements: cam_base (“CAM BASE”)
BladeStock¶
-
MillCutParameters.
BladeStock
¶ Returns the blade stock
-------------------------------------
Getter Method
Signature
BladeStock()
Returns: the blade stock builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.0.0.
License requirements: None.
BlankDistance¶
-
MillCutParameters.
BlankDistance
¶ Returns the blank distance
-------------------------------------
Getter Method
Signature
BlankDistance()
Returns: the blank distance builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
BlankOverhang¶
-
MillCutParameters.
BlankOverhang
¶ Returns the blank overhang (inheritable tool dependent).
Its relative UI name is changed to “Tool Overhang” from NX8.0. But it is named to “First Pass Overhang” in floor milling and floor and wall milling
-------------------------------------
Getter Method
Signature
BlankOverhang()
Returns: the blank overhang Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX6.0.0.
License requirements: None.
BlankStock¶
-
MillCutParameters.
BlankStock
¶ Returns the blank stock
-------------------------------------
Getter Method
Signature
BlankStock()
Returns: the stock blank builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
BlendStock¶
-
MillCutParameters.
BlendStock
¶ Returns the blend stock
-------------------------------------
Getter Method
Signature
BlendStock()
Returns: the blend stock builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.0.0.
License requirements: None.
BoundaryApproximation¶
-
MillCutParameters.
BoundaryApproximation
¶ Returns or sets the boundary approximation toggle
-------------------------------------
Getter Method
Signature
BoundaryApproximation()
Returns: the Boundary Profile Pass Flag Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BoundaryApproximation(propValue)
Parameters: propValue (bool) – the Boundary Profile Pass Flag New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
BoundaryInTol¶
-
MillCutParameters.
BoundaryInTol
¶ Returns or sets the boundary intol
-------------------------------------
Getter Method
Signature
BoundaryInTol()
Returns: the boundary intol value Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BoundaryInTol(propValue)
Parameters: propValue (float) – the boundary intol value New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
BoundaryOutTol¶
-
MillCutParameters.
BoundaryOutTol
¶ Returns or sets the boundary out tol
-------------------------------------
Getter Method
Signature
BoundaryOutTol()
Returns: the boundary out tol value Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BoundaryOutTol(propValue)
Parameters: propValue (float) – the boundary out tol value New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
BoundaryStock¶
-
MillCutParameters.
BoundaryStock
¶ Returns or sets the boundary stock
-------------------------------------
Getter Method
Signature
BoundaryStock()
Returns: the boundary stock value Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BoundaryStock(propValue)
Parameters: propValue (float) – the trim stock value New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
CheckStock¶
-
MillCutParameters.
CheckStock
¶ Returns the check stock
-------------------------------------
Getter Method
Signature
CheckStock()
Returns: The check stock builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
CleanupOutput¶
-
MillCutParameters.
CleanupOutput
¶ Returns the Cleanup Output
-------------------------------------
Getter Method
Signature
CleanupOutput()
Returns: Return type: NXOpen.CAM.CleanupOutput
New in version NX6.0.0.
License requirements: None.
CleanupSettings¶
-
MillCutParameters.
CleanupSettings
¶ Returns the Cleanup Settings
-------------------------------------
Getter Method
Signature
CleanupSettings()
Returns: Return type: NXOpen.CAM.CleanupSettings
New in version NX6.0.0.
License requirements: None.
CornerControl¶
-
MillCutParameters.
CornerControl
¶ Returns the corner control
-------------------------------------
Getter Method
Signature
CornerControl()
Returns: Return type: NXOpen.CAM.CornerControlBuilder
New in version NX6.0.0.
License requirements: None.
CornerFindingOptions¶
-
MillCutParameters.
CornerFindingOptions
¶ Returns or sets the Corner Finding Options
-------------------------------------
Getter Method
Signature
CornerFindingOptions()
Returns: the Finding Corner type Return type: NXOpen.CAM.CutParametersCornerFindingTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CornerFindingOptions(cornerFinding)
Parameters: cornerFinding ( NXOpen.CAM.CutParametersCornerFindingTypes
) – the Finding Corner typeNew in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
CutAngle¶
-
MillCutParameters.
CutAngle
¶ Returns the cut angle
-------------------------------------
Getter Method
Signature
CutAngle()
Returns: Return type: NXOpen.CAM.CutAngle
New in version NX6.0.0.
License requirements: None.
CutAreaExtensionDistance¶
-
MillCutParameters.
CutAreaExtensionDistance
¶ Returns the cut area extension distance builder
-------------------------------------
Getter Method
Signature
CutAreaExtensionDistance()
Returns: the cut area extension distance builder Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX6.0.0.
License requirements: None.
CutBelowOverhangingBlank¶
-
MillCutParameters.
CutBelowOverhangingBlank
¶ Returns or sets the Cut Below Overhanging Blank Method
-------------------------------------
Getter Method
Signature
CutBelowOverhangingBlank()
Returns: Return type: bool New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
CutBelowOverhangingBlank(propValue)
Parameters: propValue (bool) – the Cut Below Overhanging Blank Method New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
CutBelowToolContact¶
-
MillCutParameters.
CutBelowToolContact
¶ Returns or sets the cut below tool contact setting
-------------------------------------
Getter Method
Signature
CutBelowToolContact()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CutBelowToolContact(cutBelowToolContact)
Parameters: cutBelowToolContact (bool) – New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
CutBetweenLevels¶
-
MillCutParameters.
CutBetweenLevels
¶ Returns or sets the cut between levels
-------------------------------------
Getter Method
Signature
CutBetweenLevels()
Returns: the cut between method Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CutBetweenLevels(cutBetween)
Parameters: cutBetween (bool) – the cut between method New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
CutDirection¶
-
MillCutParameters.
CutDirection
¶ Returns the cut direction
-------------------------------------
Getter Method
Signature
CutDirection()
Returns: Return type: NXOpen.CAM.CutDirection
New in version NX6.0.0.
License requirements: None.
CutOrder¶
-
MillCutParameters.
CutOrder
¶ Returns or sets the cut order
-------------------------------------
Getter Method
Signature
CutOrder()
Returns: Return type: NXOpen.CAM.CutParametersCutOrderTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CutOrder(propValue)
Parameters: propValue ( NXOpen.CAM.CutParametersCutOrderTypes
) –New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
CutWallsOnly¶
-
MillCutParameters.
CutWallsOnly
¶ Returns or sets the Cut Walls Only toggle
-------------------------------------
Getter Method
Signature
CutWallsOnly()
Returns: the Cut Walls Only Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CutWallsOnly(propValue)
Parameters: propValue (bool) – the Cut Walls Only New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
ExtendAcrossUndercut¶
-
MillCutParameters.
ExtendAcrossUndercut
¶ Returns or sets the extend across undercut toggle
-------------------------------------
Getter Method
Signature
ExtendAcrossUndercut()
Returns: the Extend Across Undercut value Return type: bool New in version NX10.0.2.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
ExtendAcrossUndercut(propValue)
Parameters: propValue (bool) – the Extend Across Undercut value New in version NX10.0.2.
License requirements: cam_base (“CAM BASE”)
ExtendAtEdges¶
-
MillCutParameters.
ExtendAtEdges
¶ Returns the Extend At Edges
-------------------------------------
Getter Method
Signature
ExtendAtEdges()
Returns: Return type: NXOpen.CAM.ExtendAtEdges
New in version NX6.0.0.
License requirements: None.
ExtendFloorTo¶
-
MillCutParameters.
ExtendFloorTo
¶ Returns or sets the extend floor to
-------------------------------------
Getter Method
Signature
ExtendFloorTo()
Returns: the extend floor to option Return type: NXOpen.CAM.CutParametersExtendFloorTypes
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExtendFloorTo(option)
Parameters: option ( NXOpen.CAM.CutParametersExtendFloorTypes
) – the extend floor to optionNew in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
ExtendToPart¶
-
MillCutParameters.
ExtendToPart
¶ Returns or sets the extend to part flag
-------------------------------------
Getter Method
Signature
ExtendToPart()
Returns: the extend to part flag Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExtendToPart(flag)
Parameters: flag (bool) – the extend to part flag New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
FinishPasses¶
-
MillCutParameters.
FinishPasses
¶ Returns the finish passes
-------------------------------------
Getter Method
Signature
FinishPasses()
Returns: the finish passes builder Return type: NXOpen.CAM.FinishPassesBuilder
New in version NX6.0.0.
License requirements: None.
FloorSameAsPartStock¶
-
MillCutParameters.
FloorSameAsPartStock
¶ Returns or sets the floor same as part stock
-------------------------------------
Getter Method
Signature
FloorSameAsPartStock()
Returns: the stock part use status Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FloorSameAsPartStock(stockPartStatus)
Parameters: stockPartStatus (bool) – the stock part use status New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
FloorStock¶
-
MillCutParameters.
FloorStock
¶ Returns the floor stock
-------------------------------------
Getter Method
Signature
FloorStock()
Returns: the floor stock builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
FollowCheck¶
-
MillCutParameters.
FollowCheck
¶ Returns or sets the follow check geometry status
-------------------------------------
Getter Method
Signature
FollowCheck()
Returns: the Follow Check Geometry Status Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FollowCheck(propValue)
Parameters: propValue (bool) – the Follow Check Geometry Status New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
FromLeadingEdge¶
-
MillCutParameters.
FromLeadingEdge
¶ Returns the from leading edge
-------------------------------------
Getter Method
Signature
FromLeadingEdge()
Returns: Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX7.0.0.
License requirements: None.
FromTrailingEdge¶
-
MillCutParameters.
FromTrailingEdge
¶ Returns the from trailing edge
-------------------------------------
Getter Method
Signature
FromTrailingEdge()
Returns: Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX7.0.0.
License requirements: None.
GlobalOptimization¶
-
MillCutParameters.
GlobalOptimization
¶ Returns or sets the global optimzation status
-------------------------------------
Getter Method
Signature
GlobalOptimization()
Returns: global optimization status Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GlobalOptimization(globalOptStatus)
Parameters: globalOptStatus (bool) – global optimization status New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
HubStock¶
-
MillCutParameters.
HubStock
¶ Returns the hub stock
-------------------------------------
Getter Method
Signature
HubStock()
Returns: the hub stock builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.0.0.
License requirements: None.
IncludeBodiesOfSurfaceRegion¶
-
MillCutParameters.
IncludeBodiesOfSurfaceRegion
¶ Returns or sets the flag to check bodies of surface region
-------------------------------------
Getter Method
Signature
IncludeBodiesOfSurfaceRegion()
Returns: flag of including bodies of surface region Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IncludeBodiesOfSurfaceRegion(includeBodies)
Parameters: includeBodies (bool) – flag of including bodies of surface region New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
LevelToLevel¶
-
MillCutParameters.
LevelToLevel
¶ Returns the Level to Level
-------------------------------------
Getter Method
Signature
LevelToLevel()
Returns: Return type: NXOpen.CAM.LevelToLevel
New in version NX6.0.0.
License requirements: None.
LowerLimit¶
-
MillCutParameters.
LowerLimit
¶ Returns the lower limit
-------------------------------------
Getter Method
Signature
LowerLimit()
Returns: Return type: NXOpen.CAM.LowerLimit
New in version NX6.0.0.
License requirements: None.
MaxCutStep¶
-
MillCutParameters.
MaxCutStep
¶ Returns the maximum cut step
-------------------------------------
Getter Method
Signature
MaxCutStep()
Returns: The Max. Step Size builder Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX6.0.0.
License requirements: None.
MaxCutTraverse¶
-
MillCutParameters.
MaxCutTraverse
¶ Returns the max cut traverse
-------------------------------------
Getter Method
Signature
MaxCutTraverse()
Returns: Return type: NXOpen.CAM.MaxCutTraverse
New in version NX6.0.0.
License requirements: None.
MergeDistance¶
-
MillCutParameters.
MergeDistance
¶ Returns the merge distance builder (tool dependent double)
-------------------------------------
Getter Method
Signature
MergeDistance()
Returns: Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX6.0.0.
License requirements: None.
MinCutVolume¶
-
MillCutParameters.
MinCutVolume
¶ Returns the minimum cut volume
-------------------------------------
Getter Method
Signature
MinCutVolume()
Returns: Return type: NXOpen.CAM.MinCutVolume
New in version NX6.0.0.
License requirements: None.
MinMaterialThickness¶
-
MillCutParameters.
MinMaterialThickness
¶ Returns the minimum material thickness
-------------------------------------
Getter Method
Signature
MinMaterialThickness()
Returns: the minimum thickness builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
MinimizeNumberOfEngages¶
-
MillCutParameters.
MinimizeNumberOfEngages
¶ Returns or sets the minimize number of engages toggle
-------------------------------------
Getter Method
Signature
MinimizeNumberOfEngages()
Returns: the Minimize Number of Engages Flag Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MinimizeNumberOfEngages(propValue)
Parameters: propValue (bool) – the Minimize Number of Engages Flag New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
MultiDepthCut¶
-
MillCutParameters.
MultiDepthCut
¶ Returns the Multi Depth Cut
-------------------------------------
Getter Method
Signature
MultiDepthCut()
Returns: Return type: NXOpen.CAM.MultiDepthCut
New in version NX6.0.0.
License requirements: None.
OutputUncutRegions¶
-
MillCutParameters.
OutputUncutRegions
¶ Returns the output uncut regions
-------------------------------------
Getter Method
Signature
OutputUncutRegions()
Returns: Return type: NXOpen.CAM.OutputUncutRegions
New in version NX6.0.0.
License requirements: None.
PartStockOffset¶
-
MillCutParameters.
PartStockOffset
¶ Returns the part stock offset
-------------------------------------
Getter Method
Signature
PartStockOffset()
Returns: The Part Stock Offset builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
PatternDirection¶
-
MillCutParameters.
PatternDirection
¶ Returns or sets the pattern direction
-------------------------------------
Getter Method
Signature
PatternDirection()
Returns: Return type: NXOpen.CAM.CutParametersPatternDirectionTypes
New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
PatternDirection(propValue)
Parameters: propValue ( NXOpen.CAM.CutParametersPatternDirectionTypes
) –New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
PlungeDirection¶
-
MillCutParameters.
PlungeDirection
¶ Returns or sets the plunge direction
-------------------------------------
Getter Method
Signature
PlungeDirection()
Returns: The plunge direction Return type: NXOpen.CAM.CutParametersPlungeDirectionTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PlungeDirection(propValue)
Parameters: propValue ( NXOpen.CAM.CutParametersPlungeDirectionTypes
) – The plunge directionNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
PreventUndercutting¶
-
MillCutParameters.
PreventUndercutting
¶ Returns or sets the prevent undercutting toggle
This property is deprecated. Use
NXOpen.CAM.MillCutParameters.AllowUndercutting`()
instead.-------------------------------------
Getter Method
Signature
PreventUndercutting()
Returns: the Undercut Handle Flag Return type: bool New in version NX6.0.0.
Deprecated since version NX8.0.0: Use
NXOpen.CAM.MillCutParameters.AllowUndercutting`()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
PreventUndercutting(propValue)
Parameters: propValue (bool) – the Undercut Handle Flag New in version NX6.0.0.
Deprecated since version NX8.0.0: Use
NXOpen.CAM.MillCutParameters.AllowUndercutting`()
instead.License requirements: cam_base (“CAM BASE”)
RegionConnection¶
-
MillCutParameters.
RegionConnection
¶ Returns or sets the region connection
-------------------------------------
Getter Method
Signature
RegionConnection()
Returns: the Region Connection Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RegionConnection(propValue)
Parameters: propValue (bool) – the Region Connection New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
RegionSequencing¶
-
MillCutParameters.
RegionSequencing
¶ Returns or sets the region resequencing
-------------------------------------
Getter Method
Signature
RegionSequencing()
Returns: Return type: NXOpen.CAM.CutParametersRegionSequencingTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RegionSequencing(propValue)
Parameters: propValue ( NXOpen.CAM.CutParametersRegionSequencingTypes
) –New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
RollToolOverEdges¶
-
MillCutParameters.
RollToolOverEdges
¶ Returns or sets the roll tool over edges toggle
-------------------------------------
Getter Method
Signature
RollToolOverEdges()
Returns: the Remove Edge Traces value Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RollToolOverEdges(propValue)
Parameters: propValue (bool) – the Remove Edge Traces value New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
RotaryMaxAngleLimit¶
-
MillCutParameters.
RotaryMaxAngleLimit
¶ Returns or sets the rotary max angle limit
-------------------------------------
Getter Method
Signature
RotaryMaxAngleLimit()
Returns: the rotary max angle limit Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RotaryMaxAngleLimit(angle)
Parameters: angle (float) – the rotary max angle limit New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
RotaryMinAngleLimit¶
-
MillCutParameters.
RotaryMinAngleLimit
¶ Returns or sets the min angle from part axis
-------------------------------------
Getter Method
Signature
RotaryMinAngleLimit()
Returns: the rotary min angle limit Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RotaryMinAngleLimit(angle)
Parameters: angle (float) – the rotary min angle limit New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
SelfIntersection¶
-
MillCutParameters.
SelfIntersection
¶ Returns or sets the Standard Drive Self-Intersect Status
-------------------------------------
Getter Method
Signature
SelfIntersection()
Returns: The Standard Drive Self-Intersect Status value Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SelfIntersection(selfIntersect)
Parameters: selfIntersect (bool) – The Standard Drive Self-Intersect Status value New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
ShroudStock¶
-
MillCutParameters.
ShroudStock
¶ Returns the shroud stock
-------------------------------------
Getter Method
Signature
ShroudStock()
Returns: the shroud stock builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.0.0.
License requirements: None.
SimplifyShapes¶
-
MillCutParameters.
SimplifyShapes
¶ Returns or sets the Simplify Shapes Method
-------------------------------------
Getter Method
Signature
SimplifyShapes()
Returns: Return type: NXOpen.CAM.CutParametersSimplifyShapesTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SimplifyShapes(propValue)
Parameters: propValue ( NXOpen.CAM.CutParametersSimplifyShapesTypes
) –New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
SinglePassOffset¶
-
MillCutParameters.
SinglePassOffset
¶ Returns the Single Pass Offset
-------------------------------------
Getter Method
Signature
SinglePassOffset()
Returns: Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX8.0.0.
License requirements: None.
SmallAreaAvoidance¶
-
MillCutParameters.
SmallAreaAvoidance
¶ Returns the small area avoidance
-------------------------------------
Getter Method
Signature
SmallAreaAvoidance()
Returns: the small area builder Return type: NXOpen.CAM.SmallAreaAvoidance
New in version NX6.0.0.
License requirements: None.
SteepContainment¶
-
MillCutParameters.
SteepContainment
¶ Returns the steep containment
-------------------------------------
Getter Method
Signature
SteepContainment()
Returns: Return type: NXOpen.CAM.SteepContainment
New in version NX6.0.0.
License requirements: None.
Stepover¶
-
MillCutParameters.
Stepover
¶ Returns the stepover
-------------------------------------
Getter Method
Signature
Stepover()
Returns: Return type: NXOpen.CAM.StepoverBuilder
New in version NX6.0.0.
License requirements: None.
StepoverLimit¶
-
MillCutParameters.
StepoverLimit
¶ Returns the Stepover Limit
-------------------------------------
Getter Method
Signature
StepoverLimit()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
TextDepth¶
-
MillCutParameters.
TextDepth
¶ Returns the Text Depth
-------------------------------------
Getter Method
Signature
TextDepth()
Returns: The Text Depth builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
TlaxisBladeRollAngle¶
-
MillCutParameters.
TlaxisBladeRollAngle
¶ Returns or sets the max blade roll angle
-------------------------------------
Getter Method
Signature
TlaxisBladeRollAngle()
Returns: the max blade roll angle value Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TlaxisBladeRollAngle(angle)
Parameters: angle (float) – the max blade roll angle value New in version NX7.0.0.
License requirements: cam_base (“CAM BASE”)
TolerantMachining¶
-
MillCutParameters.
TolerantMachining
¶ Returns or sets the tolerant machining status
-------------------------------------
Getter Method
Signature
TolerantMachining()
Returns: the tolerant machining status Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TolerantMachining(tolerantMachine)
Parameters: tolerantMachine (bool) – the tolerant machining status New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
ToolAxisChange¶
-
MillCutParameters.
ToolAxisChange
¶ Returns the tool axis change
-------------------------------------
Getter Method
Signature
ToolAxisChange()
Returns: Return type: NXOpen.CAM.ToolAxisChange
New in version NX6.0.0.
License requirements: None.
ToolAxisSmoothing¶
-
MillCutParameters.
ToolAxisSmoothing
¶ Returns or sets the degree of tool axis smoothing
-------------------------------------
Getter Method
Signature
ToolAxisSmoothing()
Returns: the Smoothing value Return type: int New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToolAxisSmoothing(smoothing)
Parameters: smoothing (int) – the Smoothing value New in version NX7.0.0.
License requirements: cam_base (“CAM BASE”)
ToolAxisTilt¶
-
MillCutParameters.
ToolAxisTilt
¶ Returns the tool axis tilt
-------------------------------------
Getter Method
Signature
ToolAxisTilt()
Returns: the tool axis tilt builder Return type: NXOpen.CAM.ToolAxisTilt
New in version NX6.0.0.
License requirements: None.
ToolRunOff¶
-
MillCutParameters.
ToolRunOff
¶ Returns the Tool Run Off
-------------------------------------
Getter Method
Signature
ToolRunOff()
Returns: Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX8.0.0.
License requirements: None.
ToolRunOffType¶
-
MillCutParameters.
ToolRunOffType
¶ Returns or sets the Tool Run Off Type
-------------------------------------
Getter Method
Signature
ToolRunOffType()
Returns: the Tool Run Off type Return type: NXOpen.CAM.CutParametersToolRunOffTypes
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToolRunOffType(toolRunOff)
Parameters: toolRunOff ( NXOpen.CAM.CutParametersToolRunOffTypes
) – the Tool Run Off typeNew in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
ToolRunOn¶
-
MillCutParameters.
ToolRunOn
¶ Returns the Tool Run On
-------------------------------------
Getter Method
Signature
ToolRunOn()
Returns: Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX8.0.0.
License requirements: None.
ToolpathSmoothing¶
-
MillCutParameters.
ToolpathSmoothing
¶ Returns or sets the degree of tool path smoothing
-------------------------------------
Getter Method
Signature
ToolpathSmoothing()
Returns: the Smoothing value Return type: int New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToolpathSmoothing(smoothing)
Parameters: smoothing (int) – the Smoothing value New in version NX7.0.0.
License requirements: cam_base (“CAM BASE”)
TraverseOpenPasses¶
-
MillCutParameters.
TraverseOpenPasses
¶ Returns or sets the open passes
-------------------------------------
Getter Method
Signature
TraverseOpenPasses()
Returns: Return type: NXOpen.CAM.CutParametersTraverseOpenPassesTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TraverseOpenPasses(propValue)
Parameters: propValue ( NXOpen.CAM.CutParametersTraverseOpenPassesTypes
) –New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
TrimControl¶
-
MillCutParameters.
TrimControl
¶ Returns or sets the trim control method type
-------------------------------------
Getter Method
Signature
TrimControl()
Returns: Return type: NXOpen.CAM.CutParametersTrimControlTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TrimControl(propValue)
Parameters: propValue ( NXOpen.CAM.CutParametersTrimControlTypes
) –New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
TrimStock¶
-
MillCutParameters.
TrimStock
¶ Returns the trim stock
-------------------------------------
Getter Method
Signature
TrimStock()
Returns: the Stock of Trim Geometry builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
TrochoidalSettings¶
-
MillCutParameters.
TrochoidalSettings
¶ Returns the Trochoidal Settings
-------------------------------------
Getter Method
Signature
TrochoidalSettings()
Returns: Return type: NXOpen.CAM.TrochoidalSettings
New in version NX6.0.0.
License requirements: None.
UpDownCutting¶
-
MillCutParameters.
UpDownCutting
¶ Returns the up down cutting
-------------------------------------
Getter Method
Signature
UpDownCutting()
Returns: Return type: NXOpen.CAM.UpDownCutting
New in version NX6.0.0.
License requirements: None.
UsePrevious2dIpw¶
-
MillCutParameters.
UsePrevious2dIpw
¶ Returns or sets the use previous IPW toggle
-------------------------------------
Getter Method
Signature
UsePrevious2dIpw()
Returns: the Use Previous IPW Flag Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UsePrevious2dIpw(propValue)
Parameters: propValue (bool) – the Use Previous IPW Flag New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
ValleyOverlapDistance¶
-
MillCutParameters.
ValleyOverlapDistance
¶ Returns the valley overlap distance
-------------------------------------
Getter Method
Signature
ValleyOverlapDistance()
Returns: the valley overlap distance Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
WallStock¶
-
MillCutParameters.
WallStock
¶ Returns the wall stock
-------------------------------------
Getter Method
Signature
WallStock()
Returns: the stock wall builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
ZAxisSmoothing¶
-
MillCutParameters.
ZAxisSmoothing
¶ Returns the Z Axis Smoothing.
-------------------------------------
Getter Method
Signature
ZAxisSmoothing()
Returns: Return type: NXOpen.CAM.ZAxisSmoothing
New in version NX7.5.0.
License requirements: None.