LowerLimit Class

class NXOpen.CAM.LowerLimit

Bases: NXOpen.TaggedObject

Represents a NXOpen.CAM.LowerLimit

New in version NX6.0.0.

Properties

Property Description
Action Returns or sets the Lower Limit Action
Mode Returns or sets the Lower Limit Mode
Plane Returns or sets the Lower Limit Plane
Tag Returns the Tag for this object.

Methods

Enumerations

LowerLimitActionTypes Enumeration Available types for Lower Limit Actions
LowerLimitModeTypes Enumeration Available types for Lower Limit Mode

Property Detail

Action

LowerLimit.Action

Returns or sets the Lower Limit Action

-------------------------------------

Getter Method

Signature Action()

Returns:The Lower Limit Actions value
Return type:NXOpen.CAM.LowerLimitActionTypes

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Action(action)

Parameters:action (NXOpen.CAM.LowerLimitActionTypes) – lower limit action value

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

Mode

LowerLimit.Mode

Returns or sets the Lower Limit Mode

-------------------------------------

Getter Method

Signature Mode()

Returns:The Lower Limit Mode value
Return type:NXOpen.CAM.LowerLimitModeTypes

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Mode(mode)

Parameters:mode (NXOpen.CAM.LowerLimitModeTypes) – lower limit mode value

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

Plane

LowerLimit.Plane

Returns or sets the Lower Limit Plane

-------------------------------------

Getter Method

Signature Plane()

Returns:lower limit plane, entity type can be XFORM and PLANE
Return type:NXOpen.NXObject

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Plane(plane)

Parameters:plane (NXOpen.NXObject) – lower limit plane, entity type can be XFORM and PLANE

New in version NX7.5.0.

License requirements: cam_base (“CAM BASE”)