LowerLimitActionTypes Enumeration

NXOpen.CAM.LowerLimit.ActionTypes is an alias for NXOpen.CAM.LowerLimitActionTypes

class NXOpen.CAM.LowerLimitActionTypes

Bases: object

Available types for Lower Limit Actions

Enum Members

Enum Member Enum Member Description
NormalToPlane
normal to plane
AlongToolAxis
along tool axis
Warnings
warnings
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.