MaxCutTraverse Class¶
-
class
NXOpen.CAM.
MaxCutTraverse
¶ Bases:
NXOpen.TaggedObject
Represents a
NXOpen.CAM.MaxCutTraverse
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Distance | Returns the max cut traverse distance |
FeedOnShortMoves | Returns or sets the feed on short moves |
Tag | Returns the Tag for this object. |
Type | Returns or sets the max cut traverse type |
Methods¶
Enumerations¶
MaxCutTraverseTypes Enumeration | Available types for max cut traverse |
Property Detail¶
Distance¶
-
MaxCutTraverse.
Distance
¶ Returns the max cut traverse distance
-------------------------------------
Getter Method
Signature
Distance()
Returns: Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX6.0.0.
License requirements: None.
FeedOnShortMoves¶
-
MaxCutTraverse.
FeedOnShortMoves
¶ Returns or sets the feed on short moves
-------------------------------------
Getter Method
Signature
FeedOnShortMoves()
Returns: the max cut traverse status Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FeedOnShortMoves(propValue)
Parameters: propValue (bool) – the max cut traverse status New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
Type¶
-
MaxCutTraverse.
Type
¶ Returns or sets the max cut traverse type
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.CAM.MaxCutTraverseTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.CAM.MaxCutTraverseTypes
) –New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)