MaxCutTraverseTypes Enumeration

NXOpen.CAM.MaxCutTraverse.Types is an alias for NXOpen.CAM.MaxCutTraverseTypes

class NXOpen.CAM.MaxCutTraverseTypes

Bases: object

Available types for max cut traverse

Enum Members

Enum Member Enum Member Description
Inactive
inactive
Distance
distance
PercentToolDiameter
percent tool diameter
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.