CleanupSettings Class

class NXOpen.CAM.CleanupSettings

Bases: NXOpen.TaggedObject

Represents a NXOpen.CAM.CleanupSettings

New in version NX6.0.0.

Properties

Property Description
AutoSave Returns or sets the Auto Save, Cleanup Geometry Settings
Directional Returns or sets the Directional, Cleanup Geometry Settings
ExtraCrossDrive Returns or sets the Extra Cross Drive, Cleanup Geometry Settings
SteepAngle Returns the builder of Steep Angle, Cleanup Geometry Settings
SteepAreas Returns or sets the Steep Areas, Cleanup Geometry Settings
Tag Returns the Tag for this object.
Valleys Returns or sets the Valleys, Cleanup Geometry Settings

Methods

Property Detail

AutoSave

CleanupSettings.AutoSave

Returns or sets the Auto Save, Cleanup Geometry Settings

-------------------------------------

Getter Method

Signature AutoSave()

Returns:the AutoSave value
Return type:bool

New in version NX7.5.3.

License requirements: None.

-------------------------------------

Setter Method

Signature AutoSave(cleanupAutoSave)

Parameters:cleanupAutoSave (bool) – the AutoSave value

New in version NX7.5.3.

License requirements: cam_base (“CAM BASE”)

Directional

CleanupSettings.Directional

Returns or sets the Directional, Cleanup Geometry Settings

-------------------------------------

Getter Method

Signature Directional()

Returns:the Directional value
Return type:bool

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Directional(cleanupSettingSteepDirectional)

Parameters:cleanupSettingSteepDirectional (bool) – the Directional value

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

ExtraCrossDrive

CleanupSettings.ExtraCrossDrive

Returns or sets the Extra Cross Drive, Cleanup Geometry Settings

-------------------------------------

Getter Method

Signature ExtraCrossDrive()

Returns:the Extra Cross Drive value
Return type:bool

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

-------------------------------------

Setter Method

Signature ExtraCrossDrive(cleanupSettingExtraCrossDrive)

Parameters:cleanupSettingExtraCrossDrive (bool) – the Extra Cross Drive value

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

SteepAngle

CleanupSettings.SteepAngle

Returns the builder of Steep Angle, Cleanup Geometry Settings

-------------------------------------

Getter Method

Signature SteepAngle()

Returns:The Steep Angle builder
Return type:NXOpen.CAM.InheritableDoubleBuilder

New in version NX6.0.0.

License requirements: None.

SteepAreas

CleanupSettings.SteepAreas

Returns or sets the Steep Areas, Cleanup Geometry Settings

-------------------------------------

Getter Method

Signature SteepAreas()

Returns:the Steep Areas value
Return type:bool

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

-------------------------------------

Setter Method

Signature SteepAreas(cleanupSettingSteepAreas)

Parameters:cleanupSettingSteepAreas (bool) – the Steep Areas value

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

Valleys

CleanupSettings.Valleys

Returns or sets the Valleys, Cleanup Geometry Settings

-------------------------------------

Getter Method

Signature Valleys()

Returns:the Valleys value
Return type:bool

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Valleys(cleanupSettingDoubleContacts)

Parameters:cleanupSettingDoubleContacts (bool) – the Valleys value

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)