ToolAxisChange Class

class NXOpen.CAM.ToolAxisChange

Bases: NXOpen.TaggedObject

Represents a NXOpen.CAM.ToolAxisChange

New in version NX6.0.0.

Properties

Property Description
ExtendAtConvexCorner Returns or sets the extend at convex corner toggle
LiftAtConvexCorner Returns or sets the lift at convex corner toggle
MaxCornerAngle Returns the maximum corner angle
MaxToolAxisChange Returns the maximum tool axis change
Method Returns or sets the tool axis change method
MinToolAxisChange Returns the minimum tool axis change
Tag Returns the Tag for this object.
TiltAngle Returns the tilt angle

Methods

Enumerations

ToolAxisChangeMethodTypes Enumeration Available types for tool axis change method

Property Detail

ExtendAtConvexCorner

ToolAxisChange.ExtendAtConvexCorner

Returns or sets the extend at convex corner toggle

-------------------------------------

Getter Method

Signature ExtendAtConvexCorner()

Returns:the Extend at Convex Corner value
Return type:bool

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ExtendAtConvexCorner(propValue)

Parameters:propValue (bool) – the Extend at Convex Corner value

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

LiftAtConvexCorner

ToolAxisChange.LiftAtConvexCorner

Returns or sets the lift at convex corner toggle

-------------------------------------

Getter Method

Signature LiftAtConvexCorner()

Returns:the Lift at Convex Corner value
Return type:bool

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature LiftAtConvexCorner(propValue)

Parameters:propValue (bool) – the Lift at Convex Corner value

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

MaxCornerAngle

ToolAxisChange.MaxCornerAngle

Returns the maximum corner angle

-------------------------------------

Getter Method

Signature MaxCornerAngle()

Returns:The Max. Corner Angle builder
Return type:NXOpen.CAM.InheritableDoubleBuilder

New in version NX6.0.0.

License requirements: None.

MaxToolAxisChange

ToolAxisChange.MaxToolAxisChange

Returns the maximum tool axis change

-------------------------------------

Getter Method

Signature MaxToolAxisChange()

Returns:The Max. Tool Axis Change builder
Return type:NXOpen.CAM.InheritableDoubleBuilder

New in version NX6.0.0.

License requirements: None.

Method

ToolAxisChange.Method

Returns or sets the tool axis change method

-------------------------------------

Getter Method

Signature Method()

Returns:the value of max tool axis change
Return type:NXOpen.CAM.ToolAxisChangeMethodTypes

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Method(propValue)

Parameters:propValue (NXOpen.CAM.ToolAxisChangeMethodTypes) – the value of max tool axis change

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

MinToolAxisChange

ToolAxisChange.MinToolAxisChange

Returns the minimum tool axis change

-------------------------------------

Getter Method

Signature MinToolAxisChange()

Returns:The Min. Tool Axis Change builder
Return type:NXOpen.CAM.InheritableDoubleBuilder

New in version NX6.0.0.

License requirements: None.

TiltAngle

ToolAxisChange.TiltAngle

Returns the tilt angle

-------------------------------------

Getter Method

Signature TiltAngle()

Returns:The tile angle builder
Return type:NXOpen.CAM.InheritableDoubleBuilder

New in version NX6.0.0.

License requirements: None.