LevelToLevel Class

class NXOpen.CAM.LevelToLevel

Bases: NXOpen.TaggedObject

Represents a NXOpen.CAM.LevelToLevel

New in version NX6.0.0.

Properties

Property Description
RampAngle Returns the ramp angle
Tag Returns the Tag for this object.
Type Returns or sets the level to level type

Methods

Enumerations

LevelToLevelTypes Enumeration Available types for level to level method

Property Detail

RampAngle

LevelToLevel.RampAngle

Returns the ramp angle

-------------------------------------

Getter Method

Signature RampAngle()

Returns:the ramp angle builder
Return type:NXOpen.CAM.InheritableDoubleBuilder

New in version NX6.0.0.

License requirements: None.

Type

LevelToLevel.Type

Returns or sets the level to level type

-------------------------------------

Getter Method

Signature Type()

Returns:
Return type:NXOpen.CAM.LevelToLevelTypes

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Type(propValue)

Parameters:propValue (NXOpen.CAM.LevelToLevelTypes) –

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)