LevelToLevelTypes Enumeration

NXOpen.CAM.LevelToLevel.Types is an alias for NXOpen.CAM.LevelToLevelTypes

class NXOpen.CAM.LevelToLevelTypes

Bases: object

Available types for level to level method

Enum Members

Enum Member Enum Member Description
UseTransferMethod
Use transfer method
DirectOnPart
Direct on part
RampOnPart
Ramp on part
StaggerRampOnPart
Staggered ramp on part
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.