CutParametersToolRunOffTypes Enumeration

class NXOpen.CAM.CutParametersToolRunOffTypes

Bases: object

Available types for Tool Run Off Options

New in version NX8.0.0.

Enum Members

Enum Member Enum Member Description
ExtendToRegion
Extend To Region
Specify
Specify
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.