CutAngle Class

class NXOpen.CAM.CutAngle

Bases: NXOpen.TaggedObject

Represents a boundary cut angle ci Builder

New in version NX6.0.0.

Properties

Property Description
Tag Returns the Tag for this object.
Type Returns or sets the cut angle type
Value Returns or sets the cut angle value
Vector Returns or sets the single cut vector and two way vector

Methods

Enumerations

CutAngleTypes Enumeration Available types for cut angle type in boundary cut angle customizable item

Property Detail

Type

CutAngle.Type

Returns or sets the cut angle type

-------------------------------------

Getter Method

Signature Type()

Returns:the Cut Angle Type
Return type:NXOpen.CAM.CutAngleTypes

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Type(cutAngType)

Parameters:cutAngType (NXOpen.CAM.CutAngleTypes) – the Cut Angle Type

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

Value

CutAngle.Value

Returns or sets the cut angle value

-------------------------------------

Getter Method

Signature Value()

Returns:the Cut Angle Value
Return type:float

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Value(cutAng)

Parameters:cutAng (float) – the Cut Angle Value

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

Vector

CutAngle.Vector

Returns or sets the single cut vector and two way vector

-------------------------------------

Getter Method

Signature Vector()

Returns:the Cut Vector
Return type:NXOpen.Direction

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Vector(vector)

Parameters:vector (NXOpen.Direction) – the Cut Vector

New in version NX7.5.0.

License requirements: cam_base (“CAM BASE”)