CutAngleTypes Enumeration

NXOpen.CAM.CutAngle.Types is an alias for NXOpen.CAM.CutAngleTypes

class NXOpen.CAM.CutAngleTypes

Bases: object

Available types for cut angle type in boundary cut angle customizable item

Enum Members

Enum Member Enum Member Description
Auto
Automatic
Specify
User Defined
LongestLine
Longest Line
Vector
Vector
TwoWayVector
Two Way Vector
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.