AcrossVoids Class¶
-
class
NXOpen.CAM.
AcrossVoids
¶ Bases:
NXOpen.TaggedObject
Represents a
NXOpen.CAM.AcrossVoids
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
MinTraverseDistance | Returns the minimum traversal distance |
MotionType | Returns or sets the motion type |
Tag | Returns the Tag for this object. |
Methods¶
Enumerations¶
AcrossVoidsMotionTypes Enumeration | Available types for Across Voids Method in planar mill operation |
Property Detail¶
MinTraverseDistance¶
-
AcrossVoids.
MinTraverseDistance
¶ Returns the minimum traversal distance
-------------------------------------
Getter Method
Signature
MinTraverseDistance()
Returns: Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
MotionType¶
-
AcrossVoids.
MotionType
¶ Returns or sets the motion type
-------------------------------------
Getter Method
Signature
MotionType()
Returns: Return type: NXOpen.CAM.AcrossVoidsMotionTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MotionType(propValue)
Parameters: propValue ( NXOpen.CAM.AcrossVoidsMotionTypes
) –New in version NX6.0.0.
License requirements: None.