OutputUncutRegions Class¶
-
class
NXOpen.CAM.
OutputUncutRegions
¶ Bases:
NXOpen.TaggedObject
Represents a
NXOpen.CAM.OutputUncutRegions
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
AutoSaveBoundary | Returns or sets the auto save boundary toggle |
OverlapDistance | Returns or sets the overlap distance |
Tag | Returns the Tag for this object. |
Methods¶
Property Detail¶
AutoSaveBoundary¶
-
OutputUncutRegions.
AutoSaveBoundary
¶ Returns or sets the auto save boundary toggle
-------------------------------------
Getter Method
Signature
AutoSaveBoundary()
Returns: The Uncut output boundary value Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AutoSaveBoundary(outputBnd)
Parameters: outputBnd (bool) – The Uncut output boundary value New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
OverlapDistance¶
-
OutputUncutRegions.
OverlapDistance
¶ Returns or sets the overlap distance
-------------------------------------
Getter Method
Signature
OverlapDistance()
Returns: The Uncut Overlap Distance value Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OverlapDistance(overlapDist)
Parameters: overlapDist (float) – The Uncut Overlap Distance value New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)