CleanupOutput Class¶
-
class
NXOpen.CAM.
CleanupOutput
¶ Bases:
NXOpen.TaggedObject
Represents a
NXOpen.CAM.CleanupOutput
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
OutputType | Returns or sets the Output Type, Cleanup Geometry Output |
SteepMergeDistance | Returns the builder of Steep Merge, Cleanup Geometry Output |
SteepOverlapDistance | Returns the builder of Steep Overlap, Cleanup Geometry Output |
Tag | Returns the Tag for this object. |
ValleyMergeDistance | Returns the builder of Valley Merge, Cleanup Geometry Output |
ValleyOverlapDistance | Returns the builder of Valley Overlap, Cleanup Geometry Output |
Methods¶
Enumerations¶
CleanupOutputGeomTypes Enumeration | Available types for cleanup outputing geometry type, Cleanup Geometry Output |
Property Detail¶
OutputType¶
-
CleanupOutput.
OutputType
¶ Returns or sets the Output Type, Cleanup Geometry Output
-------------------------------------
Getter Method
Signature
OutputType()
Returns: the value of Stepover Return type: NXOpen.CAM.CleanupOutputGeomTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OutputType(cleanupOutputType)
Parameters: cleanupOutputType ( NXOpen.CAM.CleanupOutputGeomTypes
) – the value of StepoverNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
SteepMergeDistance¶
-
CleanupOutput.
SteepMergeDistance
¶ Returns the builder of Steep Merge, Cleanup Geometry Output
-------------------------------------
Getter Method
Signature
SteepMergeDistance()
Returns: The Steep Merge builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
SteepOverlapDistance¶
-
CleanupOutput.
SteepOverlapDistance
¶ Returns the builder of Steep Overlap, Cleanup Geometry Output
-------------------------------------
Getter Method
Signature
SteepOverlapDistance()
Returns: The Steep Overlap builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
ValleyMergeDistance¶
-
CleanupOutput.
ValleyMergeDistance
¶ Returns the builder of Valley Merge, Cleanup Geometry Output
-------------------------------------
Getter Method
Signature
ValleyMergeDistance()
Returns: The Valley Merge builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
ValleyOverlapDistance¶
-
CleanupOutput.
ValleyOverlapDistance
¶ Returns the builder of Valley Overlap, Cleanup Geometry Output
-------------------------------------
Getter Method
Signature
ValleyOverlapDistance()
Returns: The Steep Angle builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.