SmallAreaAvoidance Class

class NXOpen.CAM.SmallAreaAvoidance

Bases: NXOpen.TaggedObject

Represents a SmallArea Builder

New in version NX6.0.0.

Properties

Property Description
AreaSize Returns the area size
SmallAreaStatus Returns or sets the small area status
Tag Returns the Tag for this object.

Methods

Enumerations

SmallAreaAvoidanceStatusTypes Enumeration available types for Small Area Status

Property Detail

AreaSize

SmallAreaAvoidance.AreaSize

Returns the area size

-------------------------------------

Getter Method

Signature AreaSize()

Returns:the area size builder
Return type:NXOpen.CAM.InheritableToolDepBuilder

New in version NX6.0.0.

License requirements: None.

SmallAreaStatus

SmallAreaAvoidance.SmallAreaStatus

Returns or sets the small area status

-------------------------------------

Getter Method

Signature SmallAreaStatus()

Returns:
Return type:NXOpen.CAM.SmallAreaAvoidanceStatusTypes

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature SmallAreaStatus(newValue)

Parameters:newValue (NXOpen.CAM.SmallAreaAvoidanceStatusTypes) –

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)