ZAxisSmoothing Class¶
-
class
NXOpen.CAM.
ZAxisSmoothing
¶ Bases:
NXOpen.TaggedObject
Represents a
NXOpen.CAM.ZAxisSmoothing
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
Option | Returns or sets the z axis smoothing option. |
Radius | Returns the smoothing radius. |
RampAngle | Returns the ramp angle. |
Tag | Returns the Tag for this object. |
Methods¶
Enumerations¶
ZAxisSmoothingOptions Enumeration | Available options for z axis smoothing |
Property Detail¶
Option¶
-
ZAxisSmoothing.
Option
¶ Returns or sets the z axis smoothing option.
-------------------------------------
Getter Method
Signature
Option()
Returns: Return type: NXOpen.CAM.ZAxisSmoothingOptions
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Option(option)
Parameters: option ( NXOpen.CAM.ZAxisSmoothingOptions
) –New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
Radius¶
-
ZAxisSmoothing.
Radius
¶ Returns the smoothing radius.
-------------------------------------
Getter Method
Signature
Radius()
Returns: the smooothing radius builder Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX7.5.0.
License requirements: None.
RampAngle¶
-
ZAxisSmoothing.
RampAngle
¶ Returns the ramp angle.
-------------------------------------
Getter Method
Signature
RampAngle()
Returns: the ramp angle builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.5.0.
License requirements: None.