ExtendAtEdges Class¶
-
class
NXOpen.CAM.
ExtendAtEdges
¶ Bases:
NXOpen.TaggedObject
Represents a
NXOpen.CAM.ExtendAtEdges
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Distance | Returns the Extend at Edges distance |
Status | Returns or sets the extend at edges toggle |
Tag | Returns the Tag for this object. |
Methods¶
Property Detail¶
Distance¶
-
ExtendAtEdges.
Distance
¶ Returns the Extend at Edges distance
-------------------------------------
Getter Method
Signature
Distance()
Returns: Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX6.0.0.
License requirements: None.
Status¶
-
ExtendAtEdges.
Status
¶ Returns or sets the extend at edges toggle
-------------------------------------
Getter Method
Signature
Status()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Status(propValue)
Parameters: propValue (bool) – New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)