InspectionMethodBuilder Class¶
-
class
NXOpen.CAM.
InspectionMethodBuilder
¶ Bases:
NXOpen.CAM.MethodBuilder
Represents the builder for a CMM Inspection method.
To create a new instance of this class, use
NXOpen.CAM.InspectionGroupCollection.CreateInspectionMethodBuilder()
New in version NX7.0.0.
Properties¶
Property | Description |
---|---|
AdvanceAngle | Returns or sets the advance angle (degrees) |
ApproachDistance | Returns or sets the approach distance |
AxisExtrapolationMode | Returns or sets the analysis axis extrapolation mode |
CircularScan | Returns or sets a flag to indicate if scan arc is allowed |
ColorApproach | Returns or sets the color used for displaying approach elements |
ColorEntryExit | Returns or sets the color used for displaying entry and exit elements |
ColorLine | Returns or sets the color used for displaying path lines |
ColorMeasurePoint | Returns or sets the color used for displaying measured points |
ColorRetract | Returns or sets the color used for displaying retract elements |
ColorTransition | Returns or sets the color used for displaying transition elements |
CurvatureFactor | Returns or sets the curvature increase factor |
CurveScan | Returns or sets a flag to indicate if scan curve is allowed |
CutParameters | Returns the cut parameter object |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
CylinderCircleFitMode | Returns or sets the analysis cylinder/circle fitting mode |
DatumPlaneFittingMode | Returns or sets the analysis datum plane fitting mode |
DefaultOperationType | Returns or sets the default inspection operation type |
DepthDistance | Returns or sets the depth distance |
Description | Returns or sets the description |
EndDistance | Returns or sets the end point offset distance along the scan |
EndPercentage | Returns or sets the end Percentage along the scan |
EndUdeSet | Returns the end ude set |
EntryAvoidance | Returns or sets a flag to indicate if collision avoidance is required at entry |
EntryExitDistance | Returns or sets the distance from the entry or exit point to safe plane |
EntryPoint | Returns or sets a flag to indicate if an entry point is required |
EntryTransition | Returns or sets the type of entry transition |
ExitAvoidance | Returns or sets a flag to indicate if collision avoidance is required at exit |
ExitPoint | Returns or sets a flag to indicate if an exit point is required |
ExitTransition | Returns or sets the type of exit transition |
FeatureOffsetDistance | Returns or sets the offset feature distance |
InspectionMode | Returns or sets the default inspection mode |
LimitsOfSizeMode | Returns or sets the analysis limits of size fitting mode |
LineScan | Returns or sets a flag to indicate if scan line is allowed |
ManualPoint | Returns or sets a flag to indicate if manual point creation is allowed |
MaxSpacing | Returns or sets the maximum spacing between scan points |
MethodType | Returns or sets the method feature type |
MinSpacing | Returns or sets the minimum spacing between scan points |
NbScanPoints | Returns or sets the minimum number of scan points |
OffsetDistance | Returns or sets the offset distance |
OptimizationMethod | Returns or sets the optim method |
PaintDisplay | Returns the sub builder for paint display |
PathDisplay | Returns the sub builder for path display |
PathDisplayColors | Returns the sub builder for path display colors |
Pitch | Returns or sets the pitch of the Scan Helix |
PointCount | Returns or sets the number of path points |
PointHelix | Returns or sets a flag to indicate if point helix is allowed |
PointSequenceDirection | Returns or sets the point sequence start direction |
PointSequenceMode | Returns or sets the point sequence mode |
PointSequenceStart | Returns or sets the point sequence start location |
ProbeTipType | Returns or sets the preferred probe tip type |
ProfileDispositionMode | Returns or sets the analysis profile disposition fitting mode |
ReferenceFeatureMode | Returns or sets the relative measurement mode |
ReferenceFeatureOffsetDistance | Returns or sets the offset distance for relative measurement |
ReferenceFeaturePointCount | Returns or sets the number of points for relative measurement |
ReferenceFeatureZoneRadius | Returns or sets the zone radius for relative measurement |
RetractDistance | Returns or sets the retract distance |
Revolutions | Returns or sets the revolutions of the Scan Helix |
ScanCurveMode | Returns or sets the scan curve mode |
ScanForce | Returns or sets the scan force |
ScanModeType | Returns or sets the 3,5 axis scan mode type |
ScanSpeed | Returns or sets the scan speed |
SensorStrategy | Returns or sets the sensor selection strategy |
SilhouDisplay | Returns the sub builder for silhou display |
Speed | Returns or sets the default animation speed setting |
StartDistance | Returns or sets the start point offset distance along the scan |
StartEndMode | Returns or sets the scan start end mode |
StartPercentage | Returns or sets the start percentage along the scan |
StartUdeSet | Returns the start ude set |
StepSize | Returns or sets the scan step size |
StopRadius | Returns or sets the scan stop radius |
SurfaceProfileMode | Returns or sets the analysis surface profile fitting mode |
Sweep | Returns or sets the sweep of the Scan Helix |
Tag | Returns the Tag for this object. |
TiltAngle | Returns or sets the tilt angle (degrees) |
ToolDisplay | Returns the sub builder for tool display |
TurnDirection | Returns or sets the turn direction type of the Scan Helix |
TurnType | Returns or sets the turn type of the Scan Helix |
UCount | Returns or sets the number of points in U direction |
UEnd | Returns or sets the U end parameter |
UEndDeg | Returns or sets the U end degrees |
UEndDist | Returns or sets the U end distance |
UEndMode | Returns or sets the end U mode |
UEndSweep | Returns or sets the U sweep degrees |
UStart | Returns or sets the U start parameter |
UStartDeg | Returns or sets the U start degrees |
UStartDist | Returns or sets the U start distance |
UStartMode | Returns or sets the start U mode |
UStartSweep | Returns or sets the U start sweep degrees |
UVGrid | Returns or sets a flag to indicate if rectangular UV grid is allowed |
VCount | Returns or sets the number of points in V direction |
VEnd | Returns or sets the V end parameter |
VEndDeg | Returns or sets the V end degrees |
VEndDist | Returns or sets the V end distance |
VEndMode | Returns or sets the end V mode |
VEndSweep | Returns or sets the V sweep degrees |
VStart | Returns or sets the V start parameter |
VStartDeg | Returns or sets the V start degrees |
VStartDist | Returns or sets the V start distance |
VStartMode | Returns or sets the start V mode |
VStartSweep | Returns or sets the V start sweep degrees |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetCutMethod | Get cut method @return |
GetObject | Returns the object currently being edited by this builder. |
SetCutMethod | Set cut method |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
Property Detail¶
AdvanceAngle¶
-
InspectionMethodBuilder.
AdvanceAngle
¶ Returns or sets the advance angle (degrees)
-------------------------------------
Getter Method
Signature
AdvanceAngle()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AdvanceAngle(angle)
Parameters: angle (float) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ApproachDistance¶
-
InspectionMethodBuilder.
ApproachDistance
¶ Returns or sets the approach distance
-------------------------------------
Getter Method
Signature
ApproachDistance()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ApproachDistance(distance)
Parameters: distance (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
AxisExtrapolationMode¶
-
InspectionMethodBuilder.
AxisExtrapolationMode
¶ Returns or sets the analysis axis extrapolation mode
-------------------------------------
Getter Method
Signature
AxisExtrapolationMode()
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderAxisExtrapolationTypes
New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
AxisExtrapolationMode(mode)
Parameters: mode ( NXOpen.CAM.InspectionMethodBuilderAxisExtrapolationTypes
) –New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
CircularScan¶
-
InspectionMethodBuilder.
CircularScan
¶ Returns or sets a flag to indicate if scan arc is allowed
-------------------------------------
Getter Method
Signature
CircularScan()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CircularScan(circularScan)
Parameters: circularScan (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ColorApproach¶
-
InspectionMethodBuilder.
ColorApproach
¶ Returns or sets the color used for displaying approach elements
-------------------------------------
Getter Method
Signature
ColorApproach()
Returns: Return type: Id New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ColorApproach(colorApproach)
Parameters: colorApproach (Id) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ColorEntryExit¶
-
InspectionMethodBuilder.
ColorEntryExit
¶ Returns or sets the color used for displaying entry and exit elements
-------------------------------------
Getter Method
Signature
ColorEntryExit()
Returns: Return type: Id New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ColorEntryExit(colorEntryExit)
Parameters: colorEntryExit (Id) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ColorLine¶
-
InspectionMethodBuilder.
ColorLine
¶ Returns or sets the color used for displaying path lines
-------------------------------------
Getter Method
Signature
ColorLine()
Returns: Return type: Id New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ColorLine(colorLine)
Parameters: colorLine (Id) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ColorMeasurePoint¶
-
InspectionMethodBuilder.
ColorMeasurePoint
¶ Returns or sets the color used for displaying measured points
-------------------------------------
Getter Method
Signature
ColorMeasurePoint()
Returns: Return type: Id New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ColorMeasurePoint(colorMeasurePoint)
Parameters: colorMeasurePoint (Id) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ColorRetract¶
-
InspectionMethodBuilder.
ColorRetract
¶ Returns or sets the color used for displaying retract elements
-------------------------------------
Getter Method
Signature
ColorRetract()
Returns: Return type: Id New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ColorRetract(colorRetract)
Parameters: colorRetract (Id) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ColorTransition¶
-
InspectionMethodBuilder.
ColorTransition
¶ Returns or sets the color used for displaying transition elements
-------------------------------------
Getter Method
Signature
ColorTransition()
Returns: Return type: Id New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ColorTransition(colorTransition)
Parameters: colorTransition (Id) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
CurvatureFactor¶
-
InspectionMethodBuilder.
CurvatureFactor
¶ Returns or sets the curvature increase factor
-------------------------------------
Getter Method
Signature
CurvatureFactor()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CurvatureFactor(curvatureFactor)
Parameters: curvatureFactor (float) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
CurveScan¶
-
InspectionMethodBuilder.
CurveScan
¶ Returns or sets a flag to indicate if scan curve is allowed
-------------------------------------
Getter Method
Signature
CurveScan()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CurveScan(curveScan)
Parameters: curveScan (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
CylinderCircleFitMode¶
-
InspectionMethodBuilder.
CylinderCircleFitMode
¶ Returns or sets the analysis cylinder/circle fitting mode
-------------------------------------
Getter Method
Signature
CylinderCircleFitMode()
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderCylinderFittingTypes
New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
CylinderCircleFitMode(mode)
Parameters: mode ( NXOpen.CAM.InspectionMethodBuilderCylinderFittingTypes
) –New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DatumPlaneFittingMode¶
-
InspectionMethodBuilder.
DatumPlaneFittingMode
¶ Returns or sets the analysis datum plane fitting mode
-------------------------------------
Getter Method
Signature
DatumPlaneFittingMode()
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderDatumPlaneFittingTypes
New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
DatumPlaneFittingMode(mode)
Parameters: mode ( NXOpen.CAM.InspectionMethodBuilderDatumPlaneFittingTypes
) –New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DefaultOperationType¶
-
InspectionMethodBuilder.
DefaultOperationType
¶ Returns or sets the default inspection operation type
-------------------------------------
Getter Method
Signature
DefaultOperationType()
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderOperationTypes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DefaultOperationType(operationType)
Parameters: operationType ( NXOpen.CAM.InspectionMethodBuilderOperationTypes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DepthDistance¶
-
InspectionMethodBuilder.
DepthDistance
¶ Returns or sets the depth distance
-------------------------------------
Getter Method
Signature
DepthDistance()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DepthDistance(distance)
Parameters: distance (float) – New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EndDistance¶
-
InspectionMethodBuilder.
EndDistance
¶ Returns or sets the end point offset distance along the scan
-------------------------------------
Getter Method
Signature
EndDistance()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndDistance(endDistance)
Parameters: endDistance (float) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EndPercentage¶
-
InspectionMethodBuilder.
EndPercentage
¶ Returns or sets the end Percentage along the scan
-------------------------------------
Getter Method
Signature
EndPercentage()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndPercentage(endPercentage)
Parameters: endPercentage (float) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EntryAvoidance¶
-
InspectionMethodBuilder.
EntryAvoidance
¶ Returns or sets a flag to indicate if collision avoidance is required at entry
-------------------------------------
Getter Method
Signature
EntryAvoidance()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EntryAvoidance(entryAvoidance)
Parameters: entryAvoidance (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EntryExitDistance¶
-
InspectionMethodBuilder.
EntryExitDistance
¶ Returns or sets the distance from the entry or exit point to safe plane
-------------------------------------
Getter Method
Signature
EntryExitDistance()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EntryExitDistance(entryExitDistance)
Parameters: entryExitDistance (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EntryPoint¶
-
InspectionMethodBuilder.
EntryPoint
¶ Returns or sets a flag to indicate if an entry point is required
-------------------------------------
Getter Method
Signature
EntryPoint()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EntryPoint(entryPoint)
Parameters: entryPoint (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EntryTransition¶
-
InspectionMethodBuilder.
EntryTransition
¶ Returns or sets the type of entry transition
-------------------------------------
Getter Method
Signature
EntryTransition()
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderTransitionTypes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EntryTransition(entryTransition)
Parameters: entryTransition ( NXOpen.CAM.InspectionMethodBuilderTransitionTypes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ExitAvoidance¶
-
InspectionMethodBuilder.
ExitAvoidance
¶ Returns or sets a flag to indicate if collision avoidance is required at exit
-------------------------------------
Getter Method
Signature
ExitAvoidance()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExitAvoidance(exitAvoidance)
Parameters: exitAvoidance (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ExitPoint¶
-
InspectionMethodBuilder.
ExitPoint
¶ Returns or sets a flag to indicate if an exit point is required
-------------------------------------
Getter Method
Signature
ExitPoint()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExitPoint(exitPoint)
Parameters: exitPoint (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ExitTransition¶
-
InspectionMethodBuilder.
ExitTransition
¶ Returns or sets the type of exit transition
-------------------------------------
Getter Method
Signature
ExitTransition()
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderTransitionTypes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExitTransition(exitTransition)
Parameters: exitTransition ( NXOpen.CAM.InspectionMethodBuilderTransitionTypes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
FeatureOffsetDistance¶
-
InspectionMethodBuilder.
FeatureOffsetDistance
¶ Returns or sets the offset feature distance
-------------------------------------
Getter Method
Signature
FeatureOffsetDistance()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FeatureOffsetDistance(distance)
Parameters: distance (float) – New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
InspectionMode¶
-
InspectionMethodBuilder.
InspectionMode
¶ Returns or sets the default inspection mode
-------------------------------------
Getter Method
Signature
InspectionMode()
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderInspectionModes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InspectionMode(inspectionMode)
Parameters: inspectionMode ( NXOpen.CAM.InspectionMethodBuilderInspectionModes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
LimitsOfSizeMode¶
-
InspectionMethodBuilder.
LimitsOfSizeMode
¶ Returns or sets the analysis limits of size fitting mode
-------------------------------------
Getter Method
Signature
LimitsOfSizeMode()
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderLimitsOfSizeTypes
New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
LimitsOfSizeMode(mode)
Parameters: mode ( NXOpen.CAM.InspectionMethodBuilderLimitsOfSizeTypes
) –New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
LineScan¶
-
InspectionMethodBuilder.
LineScan
¶ Returns or sets a flag to indicate if scan line is allowed
-------------------------------------
Getter Method
Signature
LineScan()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LineScan(lineScan)
Parameters: lineScan (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ManualPoint¶
-
InspectionMethodBuilder.
ManualPoint
¶ Returns or sets a flag to indicate if manual point creation is allowed
-------------------------------------
Getter Method
Signature
ManualPoint()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ManualPoint(manualPoint)
Parameters: manualPoint (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
MaxSpacing¶
-
InspectionMethodBuilder.
MaxSpacing
¶ Returns or sets the maximum spacing between scan points
-------------------------------------
Getter Method
Signature
MaxSpacing()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MaxSpacing(maxSpacing)
Parameters: maxSpacing (float) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
MethodType¶
-
InspectionMethodBuilder.
MethodType
¶ Returns or sets the method feature type
-------------------------------------
Getter Method
Signature
MethodType()
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderMethodTypes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MethodType(type)
Parameters: type ( NXOpen.CAM.InspectionMethodBuilderMethodTypes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
MinSpacing¶
-
InspectionMethodBuilder.
MinSpacing
¶ Returns or sets the minimum spacing between scan points
-------------------------------------
Getter Method
Signature
MinSpacing()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MinSpacing(minSpacing)
Parameters: minSpacing (float) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
NbScanPoints¶
-
InspectionMethodBuilder.
NbScanPoints
¶ Returns or sets the minimum number of scan points
-------------------------------------
Getter Method
Signature
NbScanPoints()
Returns: Return type: int New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NbScanPoints(count)
Parameters: count (int) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
OffsetDistance¶
-
InspectionMethodBuilder.
OffsetDistance
¶ Returns or sets the offset distance
-------------------------------------
Getter Method
Signature
OffsetDistance()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OffsetDistance(offsetDistance)
Parameters: offsetDistance (float) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Pitch¶
-
InspectionMethodBuilder.
Pitch
¶ Returns or sets the pitch of the Scan Helix
-------------------------------------
Getter Method
Signature
Pitch()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Pitch(pitch)
Parameters: pitch (float) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
PointCount¶
-
InspectionMethodBuilder.
PointCount
¶ Returns or sets the number of path points
-------------------------------------
Getter Method
Signature
PointCount()
Returns: Return type: int New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointCount(pointCount)
Parameters: pointCount (int) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
PointHelix¶
-
InspectionMethodBuilder.
PointHelix
¶ Returns or sets a flag to indicate if point helix is allowed
-------------------------------------
Getter Method
Signature
PointHelix()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointHelix(pointHelix)
Parameters: pointHelix (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
PointSequenceDirection¶
-
InspectionMethodBuilder.
PointSequenceDirection
¶ Returns or sets the point sequence start direction
-------------------------------------
Getter Method
Signature
PointSequenceDirection()
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderPointSequenceDirectionTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointSequenceDirection(ptSeqDir)
Parameters: ptSeqDir ( NXOpen.CAM.InspectionMethodBuilderPointSequenceDirectionTypes
) –New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
PointSequenceMode¶
-
InspectionMethodBuilder.
PointSequenceMode
¶ Returns or sets the point sequence mode
-------------------------------------
Getter Method
Signature
PointSequenceMode()
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderPointSequenceModeTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointSequenceMode(ptSeqMode)
Parameters: ptSeqMode ( NXOpen.CAM.InspectionMethodBuilderPointSequenceModeTypes
) –New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
PointSequenceStart¶
-
InspectionMethodBuilder.
PointSequenceStart
¶ Returns or sets the point sequence start location
-------------------------------------
Getter Method
Signature
PointSequenceStart()
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderPointSequenceStartTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointSequenceStart(ptSeqStart)
Parameters: ptSeqStart ( NXOpen.CAM.InspectionMethodBuilderPointSequenceStartTypes
) –New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ProbeTipType¶
-
InspectionMethodBuilder.
ProbeTipType
¶ Returns or sets the preferred probe tip type
-------------------------------------
Getter Method
Signature
ProbeTipType()
Returns: Return type: NXOpen.CAM.InspectionMoveBuilderProbeTipTypes
New in version NX9.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProbeTipType(tipType)
Parameters: tipType ( NXOpen.CAM.InspectionMoveBuilderProbeTipTypes
) –New in version NX9.0.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ProfileDispositionMode¶
-
InspectionMethodBuilder.
ProfileDispositionMode
¶ Returns or sets the analysis profile disposition fitting mode
-------------------------------------
Getter Method
Signature
ProfileDispositionMode()
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderProfileDispositionTypes
New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProfileDispositionMode(mode)
Parameters: mode ( NXOpen.CAM.InspectionMethodBuilderProfileDispositionTypes
) –New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ReferenceFeatureMode¶
-
InspectionMethodBuilder.
ReferenceFeatureMode
¶ Returns or sets the relative measurement mode
-------------------------------------
Getter Method
Signature
ReferenceFeatureMode()
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderReferenceFeatureModeTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferenceFeatureMode(mode)
Parameters: mode ( NXOpen.CAM.InspectionMethodBuilderReferenceFeatureModeTypes
) –New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ReferenceFeatureOffsetDistance¶
-
InspectionMethodBuilder.
ReferenceFeatureOffsetDistance
¶ Returns or sets the offset distance for relative measurement
-------------------------------------
Getter Method
Signature
ReferenceFeatureOffsetDistance()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferenceFeatureOffsetDistance(distance)
Parameters: distance (float) – New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ReferenceFeaturePointCount¶
-
InspectionMethodBuilder.
ReferenceFeaturePointCount
¶ Returns or sets the number of points for relative measurement
-------------------------------------
Getter Method
Signature
ReferenceFeaturePointCount()
Returns: Return type: int New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferenceFeaturePointCount(pointCount)
Parameters: pointCount (int) – New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ReferenceFeatureZoneRadius¶
-
InspectionMethodBuilder.
ReferenceFeatureZoneRadius
¶ Returns or sets the zone radius for relative measurement
-------------------------------------
Getter Method
Signature
ReferenceFeatureZoneRadius()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferenceFeatureZoneRadius(radius)
Parameters: radius (float) – New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
RetractDistance¶
-
InspectionMethodBuilder.
RetractDistance
¶ Returns or sets the retract distance
-------------------------------------
Getter Method
Signature
RetractDistance()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RetractDistance(distance)
Parameters: distance (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Revolutions¶
-
InspectionMethodBuilder.
Revolutions
¶ Returns or sets the revolutions of the Scan Helix
-------------------------------------
Getter Method
Signature
Revolutions()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Revolutions(revolutions)
Parameters: revolutions (float) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ScanCurveMode¶
-
InspectionMethodBuilder.
ScanCurveMode
¶ Returns or sets the scan curve mode
-------------------------------------
Getter Method
Signature
ScanCurveMode()
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderScanCurveModeTypes
New in version NX7.5.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
ScanCurveMode(mode)
Parameters: mode ( NXOpen.CAM.InspectionMethodBuilderScanCurveModeTypes
) –New in version NX7.5.3.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ScanForce¶
-
InspectionMethodBuilder.
ScanForce
¶ Returns or sets the scan force
-------------------------------------
Getter Method
Signature
ScanForce()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ScanForce(force)
Parameters: force (float) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ScanModeType¶
-
InspectionMethodBuilder.
ScanModeType
¶ Returns or sets the 3,5 axis scan mode type
-------------------------------------
Getter Method
Signature
ScanModeType()
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderScanModeTypes
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ScanModeType(modeType)
Parameters: modeType ( NXOpen.CAM.InspectionMethodBuilderScanModeTypes
) –New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ScanSpeed¶
-
InspectionMethodBuilder.
ScanSpeed
¶ Returns or sets the scan speed
-------------------------------------
Getter Method
Signature
ScanSpeed()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ScanSpeed(speed)
Parameters: speed (float) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SensorStrategy¶
-
InspectionMethodBuilder.
SensorStrategy
¶ Returns or sets the sensor selection strategy
-------------------------------------
Getter Method
Signature
SensorStrategy()
Returns: Return type: NXOpen.CAM.InspectionMoveBuilderSensorStrategyTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SensorStrategy(sensorStrategy)
Parameters: sensorStrategy ( NXOpen.CAM.InspectionMoveBuilderSensorStrategyTypes
) –New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Speed¶
-
InspectionMethodBuilder.
Speed
¶ Returns or sets the default animation speed setting
-------------------------------------
Getter Method
Signature
Speed()
Returns: Return type: int New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Speed(speed)
Parameters: speed (int) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
StartDistance¶
-
InspectionMethodBuilder.
StartDistance
¶ Returns or sets the start point offset distance along the scan
-------------------------------------
Getter Method
Signature
StartDistance()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartDistance(startDistance)
Parameters: startDistance (float) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
StartEndMode¶
-
InspectionMethodBuilder.
StartEndMode
¶ Returns or sets the scan start end mode
-------------------------------------
Getter Method
Signature
StartEndMode()
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderUVModeTypes
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartEndMode(startEndMode)
Parameters: startEndMode ( NXOpen.CAM.InspectionMethodBuilderUVModeTypes
) –New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
StartPercentage¶
-
InspectionMethodBuilder.
StartPercentage
¶ Returns or sets the start percentage along the scan
-------------------------------------
Getter Method
Signature
StartPercentage()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartPercentage(startPercentage)
Parameters: startPercentage (float) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
StepSize¶
-
InspectionMethodBuilder.
StepSize
¶ Returns or sets the scan step size
-------------------------------------
Getter Method
Signature
StepSize()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StepSize(step)
Parameters: step (float) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
StopRadius¶
-
InspectionMethodBuilder.
StopRadius
¶ Returns or sets the scan stop radius
-------------------------------------
Getter Method
Signature
StopRadius()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StopRadius(radius)
Parameters: radius (float) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SurfaceProfileMode¶
-
InspectionMethodBuilder.
SurfaceProfileMode
¶ Returns or sets the analysis surface profile fitting mode
-------------------------------------
Getter Method
Signature
SurfaceProfileMode()
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderSurfaceProfileTypes
New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
SurfaceProfileMode(mode)
Parameters: mode ( NXOpen.CAM.InspectionMethodBuilderSurfaceProfileTypes
) –New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Sweep¶
-
InspectionMethodBuilder.
Sweep
¶ Returns or sets the sweep of the Scan Helix
-------------------------------------
Getter Method
Signature
Sweep()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Sweep(sweep)
Parameters: sweep (float) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
TiltAngle¶
-
InspectionMethodBuilder.
TiltAngle
¶ Returns or sets the tilt angle (degrees)
-------------------------------------
Getter Method
Signature
TiltAngle()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TiltAngle(angle)
Parameters: angle (float) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
TurnDirection¶
-
InspectionMethodBuilder.
TurnDirection
¶ Returns or sets the turn direction type of the Scan Helix
-------------------------------------
Getter Method
Signature
TurnDirection()
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderScanHelixTurnDirectionTypes
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TurnDirection(turnDirection)
Parameters: turnDirection ( NXOpen.CAM.InspectionMethodBuilderScanHelixTurnDirectionTypes
) –New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
TurnType¶
-
InspectionMethodBuilder.
TurnType
¶ Returns or sets the turn type of the Scan Helix
-------------------------------------
Getter Method
Signature
TurnType()
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderScanHelixTurnTypes
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TurnType(turnType)
Parameters: turnType ( NXOpen.CAM.InspectionMethodBuilderScanHelixTurnTypes
) –New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UCount¶
-
InspectionMethodBuilder.
UCount
¶ Returns or sets the number of points in U direction
-------------------------------------
Getter Method
Signature
UCount()
Returns: Return type: int New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UCount(uCount)
Parameters: uCount (int) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UEnd¶
-
InspectionMethodBuilder.
UEnd
¶ Returns or sets the U end parameter
-------------------------------------
Getter Method
Signature
UEnd()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UEnd(uEnd)
Parameters: uEnd (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UEndDeg¶
-
InspectionMethodBuilder.
UEndDeg
¶ Returns or sets the U end degrees
-------------------------------------
Getter Method
Signature
UEndDeg()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UEndDeg(uEnd)
Parameters: uEnd (float) – New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UEndDist¶
-
InspectionMethodBuilder.
UEndDist
¶ Returns or sets the U end distance
-------------------------------------
Getter Method
Signature
UEndDist()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UEndDist(uEnd)
Parameters: uEnd (float) – New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UEndMode¶
-
InspectionMethodBuilder.
UEndMode
¶ Returns or sets the end U mode
-------------------------------------
Getter Method
Signature
UEndMode()
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderUVModeTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UEndMode(uvMode)
Parameters: uvMode ( NXOpen.CAM.InspectionMethodBuilderUVModeTypes
) –New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UEndSweep¶
-
InspectionMethodBuilder.
UEndSweep
¶ Returns or sets the U sweep degrees
-------------------------------------
Getter Method
Signature
UEndSweep()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UEndSweep(uEnd)
Parameters: uEnd (float) – New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UStart¶
-
InspectionMethodBuilder.
UStart
¶ Returns or sets the U start parameter
-------------------------------------
Getter Method
Signature
UStart()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UStart(uStart)
Parameters: uStart (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UStartDeg¶
-
InspectionMethodBuilder.
UStartDeg
¶ Returns or sets the U start degrees
-------------------------------------
Getter Method
Signature
UStartDeg()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UStartDeg(uStart)
Parameters: uStart (float) – New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UStartDist¶
-
InspectionMethodBuilder.
UStartDist
¶ Returns or sets the U start distance
-------------------------------------
Getter Method
Signature
UStartDist()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UStartDist(uStart)
Parameters: uStart (float) – New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UStartMode¶
-
InspectionMethodBuilder.
UStartMode
¶ Returns or sets the start U mode
-------------------------------------
Getter Method
Signature
UStartMode()
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderUVModeTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UStartMode(uvMode)
Parameters: uvMode ( NXOpen.CAM.InspectionMethodBuilderUVModeTypes
) –New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UStartSweep¶
-
InspectionMethodBuilder.
UStartSweep
¶ Returns or sets the U start sweep degrees
-------------------------------------
Getter Method
Signature
UStartSweep()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UStartSweep(uStart)
Parameters: uStart (float) – New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UVGrid¶
-
InspectionMethodBuilder.
UVGrid
¶ Returns or sets a flag to indicate if rectangular UV grid is allowed
-------------------------------------
Getter Method
Signature
UVGrid()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UVGrid(uvGrid)
Parameters: uvGrid (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
VCount¶
-
InspectionMethodBuilder.
VCount
¶ Returns or sets the number of points in V direction
-------------------------------------
Getter Method
Signature
VCount()
Returns: Return type: int New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VCount(vCount)
Parameters: vCount (int) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
VEnd¶
-
InspectionMethodBuilder.
VEnd
¶ Returns or sets the V end parameter
-------------------------------------
Getter Method
Signature
VEnd()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VEnd(vEnd)
Parameters: vEnd (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
VEndDeg¶
-
InspectionMethodBuilder.
VEndDeg
¶ Returns or sets the V end degrees
-------------------------------------
Getter Method
Signature
VEndDeg()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VEndDeg(vEnd)
Parameters: vEnd (float) – New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
VEndDist¶
-
InspectionMethodBuilder.
VEndDist
¶ Returns or sets the V end distance
-------------------------------------
Getter Method
Signature
VEndDist()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VEndDist(vEnd)
Parameters: vEnd (float) – New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
VEndMode¶
-
InspectionMethodBuilder.
VEndMode
¶ Returns or sets the end V mode
-------------------------------------
Getter Method
Signature
VEndMode()
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderUVModeTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VEndMode(uvMode)
Parameters: uvMode ( NXOpen.CAM.InspectionMethodBuilderUVModeTypes
) –New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
VEndSweep¶
-
InspectionMethodBuilder.
VEndSweep
¶ Returns or sets the V sweep degrees
-------------------------------------
Getter Method
Signature
VEndSweep()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VEndSweep(vEnd)
Parameters: vEnd (float) – New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
VStart¶
-
InspectionMethodBuilder.
VStart
¶ Returns or sets the V start parameter
-------------------------------------
Getter Method
Signature
VStart()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VStart(vStart)
Parameters: vStart (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
VStartDeg¶
-
InspectionMethodBuilder.
VStartDeg
¶ Returns or sets the V start degrees
-------------------------------------
Getter Method
Signature
VStartDeg()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VStartDeg(vStart)
Parameters: vStart (float) – New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
VStartDist¶
-
InspectionMethodBuilder.
VStartDist
¶ Returns or sets the V start distance
-------------------------------------
Getter Method
Signature
VStartDist()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VStartDist(vStart)
Parameters: vStart (float) – New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
VStartMode¶
-
InspectionMethodBuilder.
VStartMode
¶ Returns or sets the start V mode
-------------------------------------
Getter Method
Signature
VStartMode()
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderUVModeTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VStartMode(uvMode)
Parameters: uvMode ( NXOpen.CAM.InspectionMethodBuilderUVModeTypes
) –New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
VStartSweep¶
-
InspectionMethodBuilder.
VStartSweep
¶ Returns or sets the V start sweep degrees
-------------------------------------
Getter Method
Signature
VStartSweep()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VStartSweep(vStart)
Parameters: vStart (float) – New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Method Detail¶
Validate¶
-
InspectionMethodBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.