InspectionMethodBuilderProfileDispositionTypes Enumeration

NXOpen.CAM.InspectionMethodBuilder.ProfileDispositionTypes is an alias for NXOpen.CAM.InspectionMethodBuilderProfileDispositionTypes

class NXOpen.CAM.InspectionMethodBuilderProfileDispositionTypes

Bases: object

the analysis profile disposition fitting type

Enum Members

Enum Member Enum Member Description
Standard
Standard
Upper
Upper
Lower
Lower
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.